Hello, I am looking to use a PowerFlex 525 drive with a 480 VAC 3 phase input, and use it to drive a 220 VAC 3 phase motor. In the manual it says the output voltage is 0 .. rated voltage. Does this mean that I can use the PowerFlex change both the voltage and the frequency? I've never done it before ...
|