Hi, I have a PF525 FW 7.0.1 with enc card with a ifm rvp510 encoder. If tried using the CCW basic wizard with enc set to single chan, once I got to the direction test part of the wizard I get 0 encoder speed with the motor moving, and when I try quadrature I get faults right away. Is there a setting ...
|