List of Contributions

mdebie

Contact Details

mdebie


My Content

1 to 10 of 10 total
Posted By mdebie Sep 25, 2024 01:08:45 AM
Found In Egroup: Advanced Software
\ view thread
Another best practice is to not synchronize all tags in the controller in your application, only the ones you need. When you synchronize tags they are all loaded in memory when the application starts so you can have a delay on startup.
Posted By mdebie Mar 22, 2024 01:58:00 AM
Found In Egroup: Advanced Software
\ view thread
Could you let us know which version you are using? I know that in 1.4 we have made a lot of improvements to the custom libraries
Posted By mdebie Oct 02, 2023 12:58:00 AM
Found In Egroup: Advanced Software
\ view thread
Which version are you using? ------------------------------ mdebie ------------------------------
Posted By mdebie Sep 18, 2023 09:57:00 AM
Found In Egroup: Advanced Software
\ view thread
This is how I set mine up. I Changed protocol from HTTPS to HTTP and the port I'm using is 8443. So when I type on my iPhone 192.168.0.17:8443 then that works for me. Maybe if you have a webbrowser open on your pc you might have to change the max connection higher than 1. ...
Posted By mdebie Sep 15, 2023 05:15:00 AM
Found In Egroup: Advanced Software
\ view thread
Hi, what are you looking for exactly? You want to connect you iPad to the Optix Runtime which is on the same network, then you just need to install the Webpresentation engine in Optix, configure it and then connect to the IP ADDRESS and Port used in the webpresentation engine. If ...
Posted By mdebie Jul 28, 2023 09:28:00 AM
Found In Egroup: Advanced Software
\ view thread
The date and time format is based on the Locale that of the currently logged in user. When you add for instance it-IT then the time format will be in 24HR. You need to add that in the setting of the project itself with Locales. The 1st one in the list is the one that also the anonymous user will ...
Posted By mdebie Jun 28, 2023 08:11:00 AM
Found In Egroup: Advanced Software
\ view thread
EDIT: Reduced the size of the images for better reading of the post -FL There isn't a widget but there is a variable available called ConnectionStatus. The easiest way is to create a label on a create, create a dynamic link and link it to the Connection Status. - ...
Posted By mdebie Jun 28, 2023 02:57:00 AM
Found In Egroup: Advanced Software
\ view thread
In the libraries there is a widget called "Station Connection Status" which uses a system tag called "Operation Code". This tag is available for most Communication stations. Below are some screenshots of the widget and also some extracts from the Optix help on how to use it and the description of ...
Posted By mdebie Jun 27, 2023 01:57:00 AM
Found In Egroup: Advanced Software
\ view thread
Have a look at the Clock Script in the Libraries : ------------------------------ mdebie ------------------------------
Posted By mdebie Jun 09, 2023 01:08:00 AM
Found In Egroup: Advanced Software
\ view thread
We use Logix Echo to communicate to FTOptix. https://www.rockwellautomation.com/en-us/products/software/factorytalk/designsuite/logix-echo.html ------------------------------ mdebie ------------------------------