List of Contributions

Baldinger

Contact Details

Baldinger


My Content

1 to 3 of 3 total
Posted By Baldinger Sep 06, 2024 06:23:12 AM
Found In Egroup: Automation Control
\ view thread
Yes, I am having the same issue with 1769-L24ER-QBFC1B using Firmware v35 after burning the SD card. I work with an OEM in control panels and have seen this a lot lately. The only way I have been able to correct this is after burning the SD card, re-download the program to the processor.
Posted By Baldinger Aug 01, 2024 09:50:35 AM
Found In Egroup: Automation Control
\ view thread
I understand there are proprietary things. I don't want specific details, just limits from series A to B I need to know if there was anything that would prevent a program from running in one or the other. I am using Studio5000 v35.
Posted By Baldinger Jul 30, 2024 02:07:00 PM
Found In Egroup: Automation Control
\ view thread
Does anyone know what the difference is with the 1769-L24ER-QBFC1B ser A and ser B? EDIT: moved to Automation Control community -Akhilesh