List of Contributions

pclancey

Contact Details

pclancey


My Content

1 to 20 of 22 total
Posted By pclancey Feb 28, 2024 02:54:00 PM
Found In Egroup: Advanced Software
\ view thread
I would like to add a string tag to hold the data server name in my @ClientTags folder, and then use it as part of the tag addressing on the HMI screen. Where I used to have as the expression for a numeric display: (/DataServer1::[PLC]SVO.ActualPosition) I would like to have: (/@ClientTags\dat ...
Posted By pclancey Feb 15, 2023 02:21:00 PM
Found In Egroup: Advanced Software
\ view thread
The push button properties pop up for me opens in the upper left, like the others: I'm in an ME project at the moment, so I don't have the same "button" object to test. Looking in an old SE project, I see what you mean, some object's property boxes open centered, others in the upper ...
Posted By pclancey Feb 15, 2023 08:25:00 AM
Found In Egroup: Advanced Software
\ view thread
If yours is centered, then mine should be able to as well. There must be a setting somewhere... which is why I posted the question. Thanks Philip. ------------------------------ pclancey ------------------------------
Posted By pclancey Feb 14, 2023 03:11:00 PM
Found In Egroup: Advanced Software
\ view thread
I am using V11, I was not clear enough in my post, sorry about that. I didn't mean the property panel on the lower right, I meant if you right click any object and select properties - the pop-up that appears is always in the upper left at location 0, 0. ------------------------------ ...
Posted By pclancey Feb 14, 2023 09:45:00 AM
Found In Egroup: Advanced Software
\ view thread
While designing in the FTV IDE, when I bring up any object's property box, FTV displays the property box in the upper left. This is a nuisance, as I am always dragging it into the middle of the screen to interact with it. Is there any way to change the default position of the FTV IDE property box? ...
Posted By pclancey Feb 10, 2022 10:07:00 AM
Found In Egroup: Advanced Software
\ view thread
Thanks for the Tech Note Daniel. The HMI alarm screens out on the production floor are all filtered to only display the alarms relevant for that area. I took one of those screens, removed all filtering, and am running it in a test client. The total number of alarms (from the status bar) hovers right ...
Posted By pclancey Feb 07, 2022 03:53:00 PM
Found In Egroup: Advanced Software
\ view thread
We have a large factory system using Logix tag based alarms, displayed in FTVSE alarm and event summary design views. By design, we do not acknowledge the alarms. They display red when they become active, green when inactive, and are sorted by event time. When a new alarm comes in, it displays in red, ...
Posted By pclancey May 03, 2019 12:13:00 PM
Found In Egroup: Advanced Software
\ view thread
Came here looking for this exact answer. How can we hide the characters being typed in a password entry string input box? SE v10 ##HL40
Posted By pclancey Apr 23, 2019 09:13:00 AM
Found In Egroup: Advanced Software
\ view thread
Summary: My time display isn't working in an existing SE v10 project because the system\Second tag is missing, and I can't add one I have system\Hour and \Minute, but no system\Second tag in my project. There are 27 system\ tags total, but no \Second. It's an existing project, already deployed, so ...
Posted By pclancey Feb 25, 2016 11:59:00 AM
Found In Egroup: Automation Control
\ view thread
Since this seems to be a bug, I called it in. Turns out someone else already did, in 10/15, but no fix yet. What causes the Color Expression to not export to .xml is only having one defined color value. In my case, there are three tags being combined, but only the value 4 was specified with a color. ...
Posted By pclancey Feb 25, 2016 08:30:00 AM
Found In Egroup: Automation Control
\ view thread
Well done, jjstraight. I didn't try importing into a new project, but I did try ctrl-A followed by ctrl-R. Sure enough, the old (no longer existing) tags are there. Soapbox mode: C'mon Rockwell, a tiny non-resizable list box for tag substitution? I get 4 lines and about 40 characters to view every ...
Posted By pclancey Feb 23, 2016 02:44:00 PM
Found In Egroup: Automation Control
\ view thread
This was exactly what I was looking for - I had seen the "cache" folder, but didn't have the courage to delete its contents. Once I closed the project, I was able to delete everything underneath it, along with the 3 files you mentioned in the "Tag" folder. I was sure this would fix the issue. ...
Posted By pclancey Feb 23, 2016 02:09:00 PM
Found In Egroup: Automation Control
\ view thread
Checking the Events was a good suggestion, I see now that a Cross Reference doesn't seem to find tags in that location. Unfortunately, I did not find the phantom tags there. I have been exporting / massaging / importing my tags multiple times as part of the SE5 - SE7 conversion, so that's not ...
Posted By pclancey Feb 22, 2016 12:38:00 PM
Found In Egroup: Automation Control
\ view thread
Summary: While testing a project that's been converted to SE7, the Client throws "failed to resolve" errors for tags that no longer exist I've been converting RSView and SE5 projects to SE7. The tag name and folder structure are being updated as part of the conversion. When I test displays with the ...
Posted By pclancey Sep 28, 2015 10:21:00 AM
Found In Egroup: Automation Control
\ view thread
Tech Support found the problem quickly - it's IE11. I uninstalled it, and now I can see my data log model tags in the configure tags dialog box. KB# 573870 has the details. ##HL40
Posted By pclancey Sep 24, 2015 12:26:00 PM
Found In Egroup: Automation Control
\ view thread
It's in the "a3" area, as opposed to the "a1" area, of this project. ##HL40
Posted By pclancey Sep 24, 2015 07:28:00 AM
Found In Egroup: Automation Control
\ view thread
Yes, the tags are visible in the model itself. I can close FTV, reboot the PC, and the tags in the data model look fine. But I can't see them in the "Configure Tags" dialog when I try to add them to a trend. I am adding a screenshot that shows the 6 tags in the data model, but the empty box from which ...
Posted By pclancey Sep 23, 2015 01:45:00 PM
Found In Egroup: Automation Control
\ view thread
Summary: There are no tags shown to pick from after selecting the Data Log Model in the Add Pens "Configure Tags" dialog I have a Data Model created with tags added. When I try to Trend one of those tags using the following steps: 1. Select Trend properties 2. Select the Pens tab ...