Vitor FIlipe Luz dos Santos
Contact Details
×
Enter Password
Enter Password
Confirm Password
Vitor FIlipe Luz dos Santos
Profile
Connections
Contacts
Contributions
Summary
Achievements
List of Contributions
My Content
1 to 5 of 5 total
search criteria =
ALL
RE: unable to switch to the new directory server because user name or password is incorrect - FactoryTalk Direct
Posted By
Vitor FIlipe Luz dos Santos
Jun 02, 2022 01:37:00 PM
Found In
Egroup:
Advanced Software
\
view thread
I have not yet tested creating a user. using the probe software i verified that most of the ports that rockwell software uses are blocked. Follow print What ports are used by the factorytalk Services platform?
RE: unable to switch to the new directory server because user name or password is incorrect - FactoryTalk Direct
Posted By
Vitor FIlipe Luz dos Santos
Jun 02, 2022 05:44:00 AM
Found In
Egroup:
Advanced Software
\
view thread
I'm typing the network administrator user in the 2 logins. The domain is in the company's domain, the user I type is the domain's network administrator.
RE: unable to switch to the new directory server because user name or password is incorrect - FactoryTalk Direct
Posted By
Vitor FIlipe Luz dos Santos
Jun 01, 2022 02:23:00 PM
Found In
Egroup:
Advanced Software
\
view thread
The computer is added. It keeps generating login failure. obs: the machine we want to configure is a VM with Win10 Enterprise Follow Photo.
RE: unable to switch to the new directory server because user name or password is incorrect - FactoryTalk Direct
Posted By
Vitor FIlipe Luz dos Santos
May 04, 2022 06:32:00 AM
Found In
Egroup:
Advanced Software
\
view thread
I've already set up the local FactoryTalk, the network is failing. The server has the correct address and running the FactoryTalkView server. I'm setting up a host for Factorytalk View studio. Do I have to add the new computer to the server administration console? Thank you.
unable to switch to the new directory server because user name or password is incorrect - FactoryTalk Direct
Posted By
Vitor FIlipe Luz dos Santos
Apr 29, 2022 11:06:00 AM
Found In
Egroup:
Advanced Software
\
view thread
I'm trying to configure a vm on the direct server, but it's generating a -unable to switch to the new directory server because user name or password is incorrect- failure. the login and password are correct, I have already tested with login and password windows administrators, already tried with local ...
Copyright � 2024 Rockwell Automation. All rights reserved.
Powered by Higher Logic