I have a customer that wants to us a non-AB PLC and control the drive on Ethernet using with the drive set up as the server and the PLC as the client. To control the speed which parameter do I write the speed to? Thanks ------------------------------ Mike Watkins ----------------------------- ...
|