Hi Raul, One basic rule of thumb that I use, when programming drives, if there are issues with the current setup, reset the parameters to default and start over. Without doing that, the drive will retain all the parameters that you have previously set up and haven't changed, and this can cause ...
|