List of Contributions

Kubilay Sezgin

Contact Details

Kubilay Sezgin


My Content

1 to 11 of 11 total
Posted By Kubilay Sezgin Jul 01, 2022 12:10:00 PM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi Alistair, It is my understanding that your supply voltage and frequency to the drive never change (400V/50Hz I believe). But, you want to send a speed command of 60Hz to the motor without changing the motor details you initially entered, this is possible. However, please bear in mind that your ...
Posted By Kubilay Sezgin Apr 29, 2022 04:11:00 AM
Found In Egroup: Automation Control
\ view thread
If I understood you correctly, the Start button that requires a confirmation is placed on a popup (the popup that is displayed after hitting a different button.). You may want to place the Start button on a screen. When it is hit, a popup with the Confirm and Cancel buttons opens. Depending on which ...
Posted By Kubilay Sezgin Apr 22, 2022 04:05:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Ahmet, Can you describe your needs more specifically? What's the application? Do you aim at point-to-point positioning? I could investigate further if I knew more details. Regards, Kubi
Posted By Kubilay Sezgin Feb 11, 2022 08:04:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Ian, Could you update the modules to the latest version (3.001)? I can't guarantee that this will fix your issue, but it's worth trying. Regards, Kubi
Posted By Kubilay Sezgin Feb 09, 2022 07:47:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Thanks for your feedback! I'll keep investigating and let you know if something comes up. Regards, Kubi
Posted By Kubilay Sezgin Feb 09, 2022 07:23:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi Ian, I asked around and found out that the same issue was experienced with the v2.01.06 of AOP (Add-on Profile) for Kinetix 5100. What's yours? The newest version (v2.01.17) is available. Regards, Kubi
Posted By Kubilay Sezgin Jan 13, 2022 07:05:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Paul, I guess that it would be possible only utilizing the Universal Feedback Board (UFB). Please see the technote below: Recommended Temposonics utilizing the PowerFlex 755 Universal Feedback Board (UFB) (custhelp.com) As for utilizing the Temposonics via Ethernet/IP, I could not ...
Posted By Kubilay Sezgin Jan 06, 2022 09:36:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Thomas, Initially, I thought that the encoder's mounted on the motor side. Quoted: "If an encoder for position/velocity accuracy is required, it is recommended to mount the encoder on the back of the motor side." Please read the knowledgebase article below: PowerFlex 525: Thoughts and ...
Posted By Kubilay Sezgin Jan 06, 2022 06:22:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
I would suggest that you perform an Auto Tune first. I guess that you want to use the "Position StepLogic" that involves a set of parameters to be configured and there is a Setup Wizard for it on CCW. You can refer to the "Appendix E" of PowerFlex 520-series user manual. 520-UM001K-EN-E PowerFlex ...
Posted By Kubilay Sezgin Dec 27, 2021 05:07:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Have you performed an Auto Tune successfully? If done properly, you may need to manually adjust the values of the following parameters 566 [Pos Reg Gain], 565 [Pos Reg Filter], 538 [Ki Speed Loop], and 539 [Kp Speed Loop]. I also suggest using the wizards on CCW (Connected Component Workbench). ...
Posted By Kubilay Sezgin Dec 22, 2021 03:22:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi - Have you tried to set P308 [Direction Mode] to 2 "Rev Disable"? What it does is that negative speed reference values are rejected and a zero speed value is used in their place. Is that what you're looking for?