List of Contributions

Wil Mattheis

Contact Details

Wil Mattheis


My Content

1 to 14 of 14 total
Posted By Wil Mattheis Apr 01, 2024 08:44:33 AM
Found In Egroup: Automation Control
\ view thread
AID QA46770 describes this anomaly. The OS version that addresses the anomaly will be included in v13 release.
Posted By Wil Mattheis Mar 01, 2024 07:44:00 AM
Found In Egroup: Automation Control
\ view thread
Hello. The only information you can access within the FT View Machine Edition application when using the TerminalInfo ActiveX control on a PC is the NIC information. This ActiveX control was designed to be used on a PanelView Plus terminal. There is also the IPInfo ActiveX control which provides only ...
Posted By Wil Mattheis Mar 24, 2023 09:14:00 AM
Found In Egroup: Automation Control
\ view thread
A couple of thoughts. First regarding the popup method, a thought was to add a numeric display to the popup as well. You can make this numeric display invisible. The first function of the numeric display is for it to capture the the Enter button press. The Enter button would contain an Event that would ...
Posted By Wil Mattheis Feb 10, 2023 07:11:00 AM
Found In Egroup: Automation Control
\ view thread
Sorry, for some reason I did not see that Phil had already responded and provided the knowbase link. My Apologies. ------------------------------ Wil Mattheis ------------------------------
Posted By Wil Mattheis Feb 10, 2023 06:59:00 AM
Found In Egroup: Automation Control
\ view thread
Hello, In the Windows 10 IoT control panel, there is a Services option (enable SFTP, VNC, etc.). One of those is also to enable the PING response. It is disabled by default. ------------------------------ Wil Mattheis ------------------------------
Posted By Wil Mattheis Feb 06, 2023 07:19:00 AM
Found In Egroup: Automation Control
\ view thread
Hello, Unfortunately, the ability to save to a network location is not supported in PanelView Plus 7 Performance series B. However, you can save to a USB flash drive or SD card. ------------------------------ Wil Mattheis ------------------------------
Posted By Wil Mattheis Feb 06, 2023 07:16:00 AM
Found In Egroup: Automation Control
\ view thread
Hello, In addition to Phil's info, I just wanted to mention that starting with FT View ME v10, you have the ability to export the Alarm History to a CSV file during runtime. I know in this case the PanelView Plus 7 is at firmware v8 but wanted to mention it for future reference. ------------------------------ ...
Posted By Wil Mattheis Jan 10, 2023 07:24:00 AM
Found In Egroup: Automation Control
\ view thread
Hello, If you are using a PanelView Plus 7 Performance series B terminal, the screen saver is currently not supported. However, you can set the screen to dim. There should be a QR code on the box the terminal came in that will take you to a document that describes some features currently not supported. ...
Posted By Wil Mattheis Nov 28, 2022 07:54:00 AM
Found In Egroup: Automation Control
\ view thread
Hello, Yes, using visibility animation and making it invisible should disable the key. ------------------------------ Wil Mattheis ------------------------------
Posted By Wil Mattheis Nov 09, 2022 07:00:00 AM
Found In Egroup: Automation Control
\ view thread
Hello, If adding a user during runtime, make sure to add the user to a Group that is defined in the runtime security settings during development (the A-P codes). There is a special button that performs the add user to a group during runtime. ------------------------------ Wil Mattheis ------ ...
Posted By Wil Mattheis Oct 04, 2022 12:28:00 PM
Found In Egroup: Automation Control
\ view thread
It will depend, but right now the CAB zip is around 180M. The recommended size of the 8G flash drive is more for when creating a backup of the terminal which is an option in the Maintenance Menu. ------------------------------ Wil Mattheis ------------------------------
Posted By Wil Mattheis Oct 04, 2022 07:34:00 AM
Found In Egroup: Automation Control
\ view thread
Hello, Which series PanelView Plus 7 do you have? Just want to confirm you are getting the correct firmware version. If you have a series B, try resetting it to Factory Default (there is a recessed button on the the logic module that will boot the PVP7 into a Maintenance Menu) and then trying it again. ...
Posted By Wil Mattheis Aug 09, 2022 06:35:00 AM
Found In Egroup: Automation Control
\ view thread
Hello, What are the date codes of the MobileView terminals?
Posted By Wil Mattheis Aug 05, 2022 07:30:00 AM
Found In Egroup: Automation Control
\ view thread
Hello, I'm not sure why your Viewpoint application is not working. Please contact Tech Support so they can start an investigation.