If the motor is already spinning when the drive gets the run command then it sounds like you need to set up flying start on P356. With flying start enabled the drive will "look" for motor RPMs then adjust output frequency to catch the motor on the fly. Yes, it is hard on the drive and motor to start ...
|