We've been having issues with drive/motor failures and I found that the VFDs were programmed as if the units were in HP rather than kW. So instead of being programmed to be 5 HP like the nameplate has, it was set to 5 kW. Could this cause any failures? ------------------------------ Carlos B. ...
|