|
150-C60NBD SMC-3, 60A, Open type enclosure, 460V, 120/240 Control This is the SMC-3 wiring diagram of from the installation manual. With 120Vac between A1-A2 and 120Vac at IN1 & IN2, the soft start should attempt to start the motor. Motor fails to Start 150-TG001 (Based on NEC Article 430) ...
|