List of Contributions

MGC

Contact Details

MGC


My Content

1 to 20 of 20 total
Posted By MGC Mar 12, 2026 06:41:28 AM
Found In Egroup: Advanced Software
\ view thread
That's perfect, thank you! -------------------------------------------
Posted By MGC Mar 12, 2026 02:51:29 AM
Found In Egroup: Advanced Software
\ view thread
That makes sense, but is there some documentation or something, where I can read about these "hidden" functions? -------------------------------------------
Posted By MGC Mar 11, 2026 12:01:00 PM
Found In Egroup: Advanced Software
\ view thread
Hi, I am using the alarm manager widget, could someone help me understand, how these links are working? As far as I can tell, when I try to add a dynamic link, the RetainedAlarms object only contains the localized alarms pointer and not these counters. I am guessing, they are added to the RetainedAlarms ...
Posted By MGC Mar 03, 2026 01:10:35 AM
Found In Egroup: Advanced Software
\ view thread
Hi! I occasionally also get this error, however, for me, it happens, if I get the "Process exceeded the timeout" warning, when the netlogic is building: 10-11-2025 09:19:32.389;WARNING;HMISolution;22e0012;Process 18204 exceeded the timeout.;; 10-11-2025 09:19:32.646;INFO;NetHelper;;User .NET solution ...
Posted By MGC Feb 26, 2026 02:48:00 AM
Found In Egroup: Advanced Software
\ view thread
Hi all, Is there a way to change the anonymous user name? My client want the default user to always be called "operator", so the user is never "anonymous". Operators should not log in. -------------------------------------------
Posted By MGC Jan 14, 2026 01:53:57 AM
Found In Egroup: Advanced Software
\ view thread
Ah, I had completely overlooked the setting to use node path in NodeIds. Thank you for your help, I got it to work now. Is there plans for function keys to be integrated into Optix in the future? -------------------------------------------
Posted By MGC Jan 14, 2026 01:12:23 AM
Found In Egroup: Advanced Software
\ view thread
Acconding to the runtime sizing tool, 1 client for the Optix server is 1 token - am I reading the sizing tool incorrectly? I did try to make the python script work, however I have not worked with the OPC server in Optix before. asemlucben do you think, you could share, how you set up the OPC UA server ...
Posted By MGC Jan 13, 2026 04:06:54 AM
Found In Egroup: Advanced Software
\ view thread
Hi Kamerling, Did you ever manage to make some function keys without a OPC server? I'm in the same situation as you were. -------------------------------------------
Posted By MGC Dec 09, 2025 02:16:26 AM
Found In Egroup: Advanced Software
\ view thread
Thank you! -------------------------------------------
Posted By MGC Dec 05, 2025 06:51:00 AM
Found In Egroup: Advanced Software
\ view thread
Hi all, I have an issue with setting a dynamic link on an object in Netlogic. I have made a type of Panel called "AI", which contains a variable called "Tag" that is a NodeId. I am attempting to make a DesignTime script, that sets a dynamic link between the "Tag" variable and a PLC tag with the following ...
Posted By MGC Sep 16, 2025 04:05:00 AM
Found In Egroup: Advanced Software
\ view thread
I found the issue, so please disregard this post. The format for DateTime is very different in the database, than when it is pulled from the database.
Posted By MGC Aug 05, 2025 01:34:40 AM
Found In Egroup: Advanced Software
\ view thread
Hi Shane, I do a remote access local connection to the optix panel from my PC, and then take a screenshot. Then I just use a graphics program (like paint 3d) to get the hex code of the color shown on the screen shot. If I do this on the emulator, the hex code is the same as the one I have input in Optix, ...
Posted By MGC Jul 28, 2025 01:28:00 AM
Found In Egroup: Advanced Software
\ view thread
Hi all, I have an issue with the OptixPanel. I have a specific color, that the customer want to use for their background. When I type in the hex code for the color on optix, and deploy to the emulator, I get the correct background color. However, when deploying the exact same project on to my OptixPanel ...
Posted By MGC Jul 28, 2025 01:27:33 AM
Found In Library: Advanced Software
Posted By MGC Jul 10, 2025 08:06:00 AM
Found In Egroup: Advanced Software
\ view thread
Ah, I was unaware, that the dynamic link was read only by default in NetLogic. Changing the link to ReadWrite fixed the issue, thank you for your help! Thanks for the tip, I'll change my naming.
Posted By MGC Jul 10, 2025 01:54:00 AM
Found In Egroup: Advanced Software
\ view thread
Hi, I am having the almost exact same issue as you, but I cannot get it to work. I am using a DesignTime netlogic to create a number of spinboxes with a respective number of buttons that have a variable, I want connected to the spinbox value. When I run the DesignTime code, the button with the dynamic ...
Posted By MGC May 28, 2025 03:42:00 AM
Found In Egroup: Advanced Software
\ view thread
Hello! I'm using optix with a Ethernet/IP connection to a Rockwell PLC, however I would like to run a secure connection between optix and the PLC, possibly CIP security. Does anyone have experience with using CIP security in optix or another secure solution? Thanks
Posted By MGC May 09, 2025 06:36:00 AM
Found In Egroup: Advanced Software
\ view thread
Thank you for your answer. I implemented the variable synchronizer as you suggested, and it works for the time being. I'm still looking info finding another way, as I potentionally have to do several of these as the project grows larger. It would be nice if there was a way to get the status of ...
Posted By MGC May 07, 2025 08:08:00 AM
Found In Egroup: Advanced Software
\ view thread
Hello everyone. I have a textbox, where I am reading a value from a PLC tag, making some calculation, and then enter the calculated value into the textbox. As the calculation is quite big and dependent on multiple different values, I am using a netlogix script, which runs when the textbox is initialized. ...
Posted By MGC Apr 29, 2025 01:55:00 AM
Found In Egroup: Advanced Software
\ view thread
Hello! I can't help with your first issue, however I had a similar issue as the second problem with the borders. As far as I can see, in 1.5 the default border thickness is 1, but in 1.6 the default border thickness has been changed to 0. I found that in 1.6, when creating a new rectangle ...