List of Contributions

Petr

Contact Details

Petr


My Content

1 to 20 of 48 total
Posted By Petr Aug 06, 2026 08:23:52 AM
Found In Egroup: Automation Control
\ view thread
Excuse me. I just wanted to know how, for example, to transfer the state of one input in PLC through the Adapter to Hilsher and vice versa, and how to set the output in PLC depending on the value in the Adapter. About Hilscher card. Hilscher support says I need two cards: one as a scanner, and the ...
Posted By Petr Aug 06, 2026 06:53:19 AM
Found In Egroup: Automation Control
\ view thread
Hello. I have another question. Is it possible to add the "ETHERNET-MODULE Generic Ethernet Module" to all controllers? We ordered the 1769-L30ER controller for testing. Does it have the ability to accept this module? Does this controller's Ethernet port support all the required exchange areas? Someone ...
Posted By Petr Aug 06, 2026 02:01:35 AM
Found In Egroup: Automation Control
\ view thread
A few more questions. How do I transfer values ​​from the controller inputs to this data exchange area (Ethernet Bridge) and vice versa? How do I write data from this area to the outputs? Will these be regular data blocks with such numbers (Assembly Instance) in the project? DataBlock(1) - Inputs ...
Posted By Petr Aug 06, 2026 01:12:41 AM
Found In Egroup: Automation Control
\ view thread
Could you please tell me more? Where did this window appear? In Studio 5000?
Posted By Petr Aug 06, 2026 12:59:41 AM
Found In Egroup: Automation Control
\ view thread
I haven't had any experience with Studio 5000. There's a lot here that's unfamiliar to me. Questions: 1. Do you use Studio 5000? 2. How did you add the ETHERNET-BRIDGE Hilsher to the Studio project? 3. Do I need to add any other hardware to the project besides the controller's hardware (I?O Configurator)? ...
Posted By Petr Aug 06, 2026 12:51:18 AM
Found In Egroup: Automation Control
\ view thread
Thank you so much. This is a really cool solution.
Posted By Petr Aug 05, 2026 01:12:29 PM
Found In Egroup: Automation Control
\ view thread
Can you tell me which organization in Germany I can contact to get a 30-day free trial for Studio 5000 Standard or Studio 5000 Professional?
Posted By Petr Aug 05, 2026 01:03:47 PM
Found In Egroup: Automation Control
\ view thread
Hello. Is it possible to download Communicatio Studio without purchasing a license? Or is downloading only available after entering the license?
Posted By Petr Aug 05, 2026 12:59:10 PM
Found In Egroup: Automation Control
\ view thread
OPC UA is very slow. There's also a way to transfer data via Node-Red.
Posted By Petr Aug 05, 2026 12:56:28 PM
Found In Egroup: Automation Control
\ view thread
To exchange data, I also need: 1. Connection name 2. config part 1 3. config part 2 (module configuration) Hilscher software here: Download Package Communication Solutions 90 - 2026-05-1 - Communication Solutions Download Package - Hilscher Confluence
Posted By Petr Aug 05, 2026 11:44:04 AM
Found In Egroup: Automation Control
\ view thread
I need to know how to create such an EDS file for exchange data in Studio 500 for Allen Bradley PLC. Then integrating it into the Hilsher project will not be difficult. Or suggest other options. I really need it. Thanks in advance.
Posted By Petr Aug 05, 2026 11:43:11 AM
Found In Egroup: Automation Control
\ view thread
I need to know how to create such an EDS file for exchange data in Studio 500 for Allen Bradley PLC. Then integrating it into the Hilsher project will not be difficult. Or suggest other options. I really need it. Thanks in advance.
Posted By Petr Aug 05, 2026 11:36:32 AM
Found In Egroup: Automation Control
\ view thread
There's a SCADA system-a computer application. This application controls the operation of various equipment. The computer application reads inputs from the peripherals and sets the peripheral outputs based on the operating algorithm. The peripherals are controlled by a Hilscher card. The API function ...
Posted By Petr Aug 05, 2026 11:26:20 AM
Found In Egroup: Automation Control
\ view thread
I need to integrate the Allen Bradley controller as an Adapter in a Hilscher project (Hilscher CFIX card is Master). How can I create an adapter for a different network in the Allen Bradley controller? For example in Hilscher software.
Posted By Petr Aug 05, 2026 11:14:19 AM
Found In Egroup: Automation Control
\ view thread
The Hilscher card is a Master (Scanner), since the Scada system on the computer controls the operation of the peripherals.
Posted By Petr Aug 05, 2026 09:08:04 AM
Found In Egroup: Automation Control
\ view thread
Protocol - EtnernetIP Data - 50 bytes for inputs and 50 bytes for outputs. Exchange time no more than 100 milliseconds. Data exchange with Hilscher CIFH card and AllenBradley CPU.
Posted By Petr Aug 05, 2026 09:02:11 AM
Found In Egroup: Automation Control
\ view thread
Thanks for the explanation. I have a few questions: Can I insert Generic Ethernet Module ? Can I write and read data from Generic Ethernet Module ? Is it possible to provide an example of parameterization of this module? Can I transfer this Generic Ethernet Module to another manufacturer's project as ...
Posted By Petr Aug 05, 2026 05:47:14 AM
Found In Egroup: Automation Control
\ view thread
I would like to insert the Allen Bradley Controller as a Generic Ethernet Module into another manufacturer's project if possible. But I need to know how to form the required fields in the Allen Bradley controller for this desigion for example. Maybe there are other ways. I wanted to know about them ...