List of Contributions

Platten

Contact Details

Platten


My Content

1 to 20 of 50+ total
Posted By Platten Feb 20, 2026 08:03:00 AM
Found In Egroup: Advanced Software
\ view thread
I am trying to populate a display in Optix. I have set-up a display adding a variable called vIOPath, this is of type String, the value assigned to this is 'Local:1:I', in C# I have added a Runtime NetLogic module which I've called 'clsGlue', this is the source code: //----------------------------- ...
Posted By Platten Feb 20, 2026 05:59:11 AM
Found In Egroup: Advanced Software
\ view thread
The SVG is now dynamically created. You cannot generalise on what you think it contains or its purpose as you haven't been given enough information. ------------------------------ Kind regards, Simon Platten ------------------------------
Posted By Platten Feb 20, 2026 02:26:00 AM
Found In Egroup: Advanced Software
\ view thread
I realise that much, the question is with the absence of any reference documentation, how? I cannot use the Auto feature it isn't present in an SVG document which is where I need to create the background rectangle. ------------------------------ Kind regards, Simon Platten ----------------- ...
Posted By Platten Feb 20, 2026 01:51:00 AM
Found In Egroup: Advanced Software
\ view thread
Shame, do you know if I can get average character width for a specific font? ------------------------------ Kind regards, Simon Platten ------------------------------
Posted By Platten Feb 20, 2026 12:56:00 AM
Found In Egroup: Advanced Software
\ view thread
I'm working on a C# API, I have a function that creates a Panel and adds an SVG that is used as the Panel backdrop, part of this will include a Title which I want to ensure that the Title has a background rectangle that clears content under the title. Is there any API function that returns the bounding ...
Posted By Platten Feb 19, 2026 01:21:15 AM
Found In Egroup: Advanced Software
\ view thread
Thank you, I will take a look. ------------------------------ Kind regards, Simon Platten ------------------------------
Posted By Platten Feb 19, 2026 01:00:55 AM
Found In Egroup: Advanced Software
\ view thread
To be honest, there is nothing to share, presently panels in Optix have no window dressing they are just containers, I want to create panels that look like panels and each has a 3D border on it with a Panel Title embedded top left in the border. Without drawing this by hand I want to use the C# to add ...
Posted By Platten Feb 19, 2026 12:44:14 AM
Found In Egroup: Advanced Software
\ view thread
The SVG size is set in the file itself, the path element does not accept % values, it takes absolutes, so it needs adjusting in order to fit. Specifically I want to create a panel background with decorative 3D borders, I was thinking that the easiest way to do this would be to use SVG? ----------- ...
Posted By Platten Feb 18, 2026 08:59:26 AM
Found In Egroup: Advanced Software
\ view thread
Is re-writing it to disk going to be effective? Isn't the SVG loaded at runtime? Can I modify the runtime version in anyway? ------------------------------ Kind regards, Simon Platten ------------------------------
Posted By Platten Feb 18, 2026 08:51:02 AM
Found In Egroup: Advanced Software
\ view thread
Yes, I am working in DesignTime, I need to modify the SVG so that it fits into the layout it is being used in. ------------------------------ Kind regards, Simon Platten ------------------------------
Posted By Platten Feb 18, 2026 08:30:00 AM
Found In Egroup: Advanced Software
\ view thread
This is very much a work in progress, I have an SVG template that I'm creating: .tb ( stroke:#ffffff; stroke-width: 3; ) The above is no-where near finished, I'm just testing things out, the macros which I want to replace are indicated by '(Height)' and '(Width)', in ...
Posted By Platten Feb 17, 2026 07:50:00 AM
Found In Egroup: Advanced Software
\ view thread
Thank you, will take a look. [Edit] I just did this for "String formatter", in Optix I right clicked the "Converters" folder and selected New then "String formatter", this adds $ StringFormatter1 to the Converters folder, double clicking it does nothing and right clicking it shows the original context ...
Posted By Platten Feb 17, 2026 07:14:00 AM
Found In Egroup: Advanced Software
\ view thread
I am working with FTOptix 1.7.0.804, porting an application from PanelView, there are a lot of things I would like to learn more about, can anyone point me to a good source of information where I can find out more, for example yesterday I discovered the Key-value Converter and very useful it is too. ...
Posted By Platten Feb 16, 2026 12:51:26 AM
Found In Egroup: Advanced Software
\ view thread
Thank you, but I need to specify the decimal precision. ------------------------------ Kind regards, Simon Platten ------------------------------
Posted By Platten Feb 13, 2026 06:27:00 AM
Found In Egroup: Advanced Software
\ view thread
I'm working on converting a project from PanelView to FTOptix, in the PanelView project there is a Line using the LineStyle Dash-Dot. I couldn't see a Line in FTOptix, but there is a PolyLine, I have opened the C# class file PolyLine (decompiled), however I cannot see a LineStyle or anything similar, ...
Posted By Platten Feb 13, 2026 05:20:00 AM
Found In Egroup: Advanced Software
\ view thread
I am porting an application (trying) from PanelView to FTOptix. In PanelView a tag is used as an index to get corresponding text, the closet thing I've found in FTOptix is the List box control, the question is how to I add text items to the List box, can this be done via the FTOptix user interface? ...
Posted By Platten Feb 13, 2026 04:11:00 AM
Found In Egroup: Advanced Software
\ view thread
I have a Complex Dynamic Link in a label: Expression: (((0)*((1)*(2))):n0) (0) Dynamic link: /Objects/Interpack2026_21166_FT140_V00_02/CommDrivers/RAEtherNet_IPDriver1/RAEtherNet_IPStation1/Tags/Program&:EM_iTrakFwInfeed/HMI_WorkingData/DeliveryQDecel_mmss (1) Dynamic link: /Obj ...
Posted By Platten Feb 13, 2026 03:10:00 AM
Found In Egroup: Advanced Software
\ view thread
I realise now that what I was seeing was a summary of all the tags utilised in the select group and by its children. I have now resolved this issue. ------------------------------ Kind regards, Simon Platten ------------------------------
Posted By Platten Feb 13, 2026 02:57:00 AM
Found In Egroup: Advanced Software
\ view thread
In a PanelView (15.00.00 (CPR 9 SR 15)), showing in the Tag Substitution dialog there is: (::[FW]Program:EM_FlowWrapper.HMI_WorkingData.McGeometry.WebJoinToKnockDown) (::[FW]Program:Un_Machine.HMI_DisplayData.NotStoppedParamLock) 1 The first two lines are links to PLC tags. I can see from starting ...
Posted By Platten Feb 13, 2026 01:30:00 AM
Found In Egroup: Advanced Software
\ view thread
Found the problem, in order to display the changes I added the screen to the MainWindow and this is where the missing row was present. Strange in that any changes I make to the original location would be mirrored in the copy that was present in the MainWindow, but changing the copy does not have the ...