List of Contributions

Aldair Ribeiro

Contact Details

Aldair Ribeiro


My Content

1 to 20 of 20 total
Posted By Aldair Ribeiro Jan 07, 2026 08:48:00 AM
Found In Egroup: Advanced Software
\ view thread
I'm trying to update the firmware package of a 6300T-BA thin client that was on version 9.5 because the Thin Manager version is 14.01 build 14000. I downloaded the package from the Thin Manager website. I installed it, but I noticed that it doesn't update the bootloader version. When the thin client ...
Posted By Aldair Ribeiro Oct 30, 2025 08:58:00 AM
Found In Egroup: Advanced Software
\ view thread
Hello, good morning! In an environment with 2 redundant SCADA servers, using the same server for the Thin Manager and having 12 thin clients connected, do I need to install 12 CALs on each server or just 12 on one of them? Regards, -------------------------------------------
Posted By Aldair Ribeiro Sep 08, 2025 06:22:00 AM
Found In Egroup: Advanced Software
\ view thread
I'm having a problem with Thin Manager v13.2 on Windows Server 2012. ThinServer is running, and my 9 clients are connected. However, I can't open the Thin Manager interface. It opens, but then freezes, and I can't do anything else. I noticed that the Thin Module is consuming 7GB of memory. Is there ...
Posted By Aldair Ribeiro Sep 05, 2025 07:37:09 AM
Found In Egroup: Advanced Software
\ view thread
Thanks Adam, greetings from Brazil! Since it's compatible with Server 2022, is that a guarantee that it will be compatible with 2025? Apparently, Rockwell hasn't declared compatibility yet.-------------------------------------------
Posted By Aldair Ribeiro Sep 03, 2025 06:10:00 AM
Found In Egroup: Advanced Software
\ view thread
I currently have Thin Manager V13.2 running on Windows Server 2012 Foundation with 15 clients. We're replacing this server with one running Windows Server 2025 Standard. I haven't found any Rockwell documentation that mentions compatibility between the two. Has anyone used it? -------------------- ...
Posted By Aldair Ribeiro Oct 14, 2024 07:28:00 AM
Found In Egroup: Installation & Activation
\ view thread
I'm trying to install Connected Components Workbench V22 and the installation won't go beyond 15% (starting the Microsoft Visual Studio 2015 Shell installer). Does anyone have a solution? Another question... I need to program a 2080-L50E24QBB. Before installing V22 I tried V12 and there was no option ...
Posted By Aldair Ribeiro Jul 24, 2024 04:14:24 PM
Found In Library: Automation Control
Posted By Aldair Ribeiro Jul 24, 2024 04:14:00 PM
Found In Egroup: Automation Control
\ view thread
Hello! I have a 1794-IE8H module controlled by a 1756-L71 and 1794-AENTR CPU. I want to read the signal from a pressure sensor that transmits 4-20 mA. However, I would like to obtain maximum resolution from the module - the application is measuring the level of a tank per column. - for this I configured ...
Posted By Aldair Ribeiro Jun 24, 2024 07:13:00 AM
Found In Egroup: Advanced Software
\ view thread
Good morning! I have two servers SLK1500P and SLK1500S both are on the same network and run Windows server 2012 Foundation. On the SLK1500P I have 9 thin clients connected and running perfectly. I'm trying to enable redundancy and the message "RPC server is not available" error "800706ba" appears. ...
Posted By Aldair Ribeiro Jun 10, 2024 11:32:00 AM
Found In Egroup: Advanced Software
\ view thread
I have 8 thin clients connected to my server and managed through thin manager. After activating the screen saver I noticed that communication was unstable, the error log shows several communication losses. By removing the screen module the problem was removed, however it is an animation that agreed with ...
Posted By Aldair Ribeiro Aug 18, 2023 03:11:22 PM
Found In Library: Networks
Posted By Aldair Ribeiro Aug 18, 2023 03:11:00 PM
Found In Egroup: Networks
\ view thread
I am sending print of ENI Utility ------------------------------ Aldair Ribeiro ------------------------------
Posted By Aldair Ribeiro Aug 18, 2023 03:10:00 PM
Found In Egroup: Networks
\ view thread
Hello Ryan! 1-I'm trying both google chrome and internet explorer (MS edge) . 2-The TX/RX light blinks normally at high frequency. 3-I'm just turning off the ENI. 4-The firmware version is already 3.22. In a last test carried out today I noticed that the direct communication ...
Posted By Aldair Ribeiro Aug 17, 2023 06:33:00 AM
Found In Egroup: Networks
\ view thread
Edited to translate into English. Please post in English going forward. @Aldair Ribeiro. Thank you. -EF EDIT: corrected Original Message View by HTML source code -FL No parameters are shown on the webpage and I also don't have access to the error log as shown in the manual. - ...
Posted By Aldair Ribeiro Aug 17, 2023 06:32:00 AM
Found In Egroup: Networks
\ view thread
------------------------------ Aldair Ribeiro ------------------------------
Posted By Aldair Ribeiro Aug 17, 2023 06:32:00 AM
Found In Egroup: Networks
\ view thread
------------------------------ Aldair Ribeiro ------------------------------
Posted By Aldair Ribeiro Aug 17, 2023 06:29:00 AM
Found In Egroup: Networks
\ view thread
Edit: Translated to English to give Aldair the best chance of getting a solution to the question. -EF Good morning! I have a NET-ENI gateway connected to the DF1 port of an SLC 5/03 cpu and connected on the ethernet side to a switch, ihm and L71. Quite often communication is lost, ...
Posted By Aldair Ribeiro May 19, 2023 07:24:00 AM
Found In Egroup: Legacy
\ view thread
Edit: Translated into English to ensure the best likelihood of getting responses. -EF EDIT: moved to Legacy community -FL Hello good morning, I need to exchange information between a CPU SLC 500 5/03 and a controllogix 1756-L71. I have a 1761-NET-ENI Gateway on the RS232 port of the SLC. ...
Posted By Aldair Ribeiro Jul 29, 2022 06:31:00 AM
Found In Egroup: Networks
\ view thread
The 1794-aentr revision is 1016, but I saw that rockwell has already released version 1022, is there any fix for this problem in this new revision?
Posted By Aldair Ribeiro Jul 27, 2022 07:37:00 PM
Found In Egroup: Networks
\ view thread
Translated text to English to give Aldair a better chance of getting the question answered. -EF ------ Hello ‎ ‎I have 5 1794-AENTR that communicate with a redundant L71 CPU via a 1756-EN2TP module. And also with 8 powerflex 753 using 20-750-ENETR. ‎ ‎I have cisco switch manageable (IE3300-8T2S) ...