List of Contributions

GLaDOS

Contact Details

GLaDOS


My Content

1 to 20 of 50+ total
Posted By GLaDOS Dec 16, 2025 08:48:54 AM
Found In Egroup: Automation Control
\ view thread
Ihor, If have the "Details Pane" option visible for your "Alarm and Even Summary" object, this value is shown for every device alarm in the details pane: ------------------------------ If you answer my questions there will be cake. ------------------------------
Posted By GLaDOS Dec 12, 2025 10:49:58 AM
Found In Egroup: Automation Control
\ view thread
Mir, I'm sure the challenges vary based upon each migration, but in my experience the main difficulty is making sure all the code in the legacy system is understood. SLC systems don't keep comments and descriptors in the PLC, so these are often lost, and it is common to encounter out of date electrical ...
Posted By GLaDOS Dec 11, 2025 08:41:27 AM
Found In Egroup: General Discussions
\ view thread
Central Wisconsin, United States ------------------------------ If you answer my questions there will be cake. ------------------------------
Posted By GLaDOS Dec 10, 2025 03:46:05 PM
Found In Egroup: Advanced Software
\ view thread
Babu, Could you share the actual errors you are getting from the diagnostic list as well? It is difficult to say what to do without knowing exactly how the passed parameters are trying to be used and what the exact error is. I assume you are trying to do some animation based upon the alarm class. ...
Posted By GLaDOS Dec 10, 2025 03:06:04 PM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Onayli, Thank you for uploading the parameter file. I would continue to suggest that the long decel time may be due to Bus regulation as you are using frequency adjustment for BUS regulation which is normal. I'm not sure there is anything programmatically you can do about that. You may have to install ...
Posted By GLaDOS Dec 08, 2025 09:54:05 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Onayli, Someone had a similar issue recently here: Powerflex 753 PTP mode decel time problem Quite frankly though, I'm not sure if their issue is resolved, but you could look at the technotes in that post and see if anything helps you. One thing to note regarding your t1-t3 and t3-t4 times is that ...
Posted By GLaDOS Dec 08, 2025 09:19:52 AM
Found In Egroup: Automation Control
\ view thread
Bruce, No, the 5370 and the 5380 models do not have a replaceable battery. ------------------------------ If you answer my questions there will be cake. ------------------------------
Posted By GLaDOS Dec 05, 2025 08:57:00 AM
Found In Egroup: Automation Control
\ view thread
Splash, It's interesting that the AOP won't open only on drives 1 & 2. It should be the same AOP as the Datalink is just an option within the AOP, not something from a separate AOP. Have you tried using CCW? I've had powerflex syncing issues with Studio 5000 before, and I got around it by simply changes ...
Posted By GLaDOS Dec 04, 2025 02:10:57 PM
Found In Egroup: Automation Control
\ view thread
Burch, I haven't done this (on the Engage forum anyway) before, and I hope you don't mind, but I like trying problems with LLM's occasionally and I thought yours was an interesting fit particularly since you provided a corrupt data file as LLM's typically excel when it comes to actual data. So I let ...
Posted By GLaDOS Dec 04, 2025 09:57:57 AM
Found In Egroup: Advanced Software
\ view thread
Minato, I don't think there is any hard tag limit with the EECM, nor is there one with FactoryTalk Optix which supplies the OPC functionality to the EECM. Obviously though, there will be some practical performance limit, but again I don't think there is any specific numbers to be given here unless ...
Posted By GLaDOS Dec 04, 2025 09:15:30 AM
Found In Egroup: Automation Control
\ view thread
BWilken, This is probably the document you need: ControlLogix SIL 2 Applications Generally speaking, changing out the PLC shouldn't be an issue in maintaining a SIL 2 rating, the 1756-L7x are all SIL 2 certified. I think the real concern would be potential IO and wiring configuration changes. The ...
Posted By GLaDOS Dec 04, 2025 07:30:00 AM
Found In Egroup: Advanced Software
\ view thread
Platten, Yes, it's configuration and/or diagnostic data. ------------------------------ If you answer my questions there will be cake. ------------------------------
Posted By GLaDOS Dec 04, 2025 07:21:28 AM
Found In Egroup: Automation Control
\ view thread
Peter, Does this help? Signaling Specifications It lists nominal current on page 23, not technically max current, but it's all I could see. ------------------------------ If you answer my questions there will be cake. ------------------------------
Posted By GLaDOS Dec 03, 2025 03:07:31 PM
Found In Egroup: Installation & Activation
\ view thread
Xie, I don't think you need to delete it, it might be useful to someone else in the future. I would just reply to yourself with the solution and mark your reply as the best answer. ------------------------------ If you answer my questions there will be cake. ------------------------------
Posted By GLaDOS Dec 03, 2025 03:05:00 PM
Found In Egroup: Automation Control
\ view thread
Vinny, Default install location of fonts should be: C:\Program Files (x86)\Rockwell Automation\CCW\PVcRuntime\Fonts Just delete the ones you don't want from the folder. ------------------------------ If you answer my questions there will be cake. ------------------------------
Posted By GLaDOS Dec 02, 2025 02:08:18 PM
Found In Egroup: Automation Control
\ view thread
Ryan, Factorytalk Design Workbench is intended to be the software for the micro 800 controllers going forward, at least those with ethernet communications, and although I haven't heard this explicitly, I imagine all the 800 models will be sold with ethernet capability eventually anyway. Other models ...
Posted By GLaDOS Nov 26, 2025 12:13:45 PM
Found In Egroup: Networks
\ view thread
Mahon, The only way to tell if the 1783-NATR is allowing communication is to open the setup and see, you can find the manual for the device here: Configurable NAT Router. I've configured these before, and haven't had any issues although it is important to remember the NAT router will need it's own ...
Posted By GLaDOS Nov 25, 2025 06:36:00 PM
Found In Egroup: Legacy
\ view thread
Patrick, The MAC address is fixed and is assigned at the factory. I don't think there is anyway to overwrite or change the MAC address as it's stored on the hardware not RSLogix software. When you download and go online the RSLogix software should read the hardware address and show whatever it is. ...
Posted By GLaDOS Nov 25, 2025 11:41:10 AM
Found In Egroup: Automation Control
\ view thread
Although it's fairly rare that I use (or come across) security setups with PLC files, my understanding was that you could indeed secure Studio 5000 projects even to prevent upload or download of the project files, or at the very least be unable to open the project file thus preventing changes or downloads ...
Posted By GLaDOS Nov 25, 2025 09:48:32 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Emre, Unfortunately, I don't see anything explicitly wrong with your parameter file. However, I did find some technotes which may be helpful. The first technote actually points out a bug that exists in firmware v12 that causes issues with accel and decel times although it's rather vague on what the ...