List of Contributions

aOptixUser

Contact Details

aOptixUser


My Content

1 to 18 of 18 total
Posted By aOptixUser Jul 31, 2026 01:28:23 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Many thanks you saved my day :)
Posted By aOptixUser Jul 30, 2026 09:24:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hello, dear community, the image below shows how we defined TagBasedAlarms in a project. How can I read or evaluate the AssociatedTags in Optix at runtime? We want to use this tag to implement FirstFaultDetection, which worked up until Optix version 1.7. Unfortunately, I can no longer find a ...
Posted By aOptixUser Jul 07, 2026 06:29:31 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Okay, I tried again. This time, I'm getting the following log message. But I don't understand this message, and I can't find any documentation about it either.
Posted By aOptixUser Jul 06, 2026 11:59:47 PM
Found In Egroup: FactoryTalk Optix
\ view thread
Sorry for my late reply, i would try it. Thanks for helping ^^
Posted By aOptixUser Jul 02, 2026 03:28:50 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Thanks for the quick reply :) We tried again, but the result is still the same. Optix Studio shows that the provider is unavailable. We also tried using different URLs, but the result is always the same. So, when we followed the instructions from Bitbucket and entered the URL shown in the image ...
Posted By aOptixUser Jul 02, 2026 01:23:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hello, everyone. I have a question about version control using the cloud version of Bitbucket. We'd like to manage the project using Bitbucket as a cloud solution. However, in the settings, we can only find the on-premises option. Is there a workaround that would allow us to use Bitbucket (Cloud) ...
Posted By aOptixUser May 19, 2026 12:14:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi Gerdes, I'm not sure if this matches your problem, but we once had a similar issue in our project. Do you have NodePointers or aliases with a specified child on the objects you want to copy? If so, this can also cause problems because the types specified on the child are copied along with ...
Posted By aOptixUser May 07, 2026 12:48:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hey Paul, did you add the X button yourself, or are you referring to the X button in the runtime window? If you added the X button yourself to close the runtime, you can use a so-called Formatted Dynamic Link to control the button's visibility property. With this, you can target specific user ...
Posted By aOptixUser Apr 22, 2026 12:22:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hey Retzlaff, Do you only want to display this number? If you only want to display this number, you can do so using an ExpressionEvaluator: Expression: "(PLC_Value)/100". Alternatively, you can cast your integer to a float using an ExpressionEvaluator: Expression: "(float)PLC_Value". ...
Posted By aOptixUser Apr 10, 2026 05:05:00 AM
Found In Egroup: Advanced Software
\ view thread
Hey Wrage, welcome here :) Which container do you use ? In case you are using the AlarmHistoryGrid from the Library, there is an "Auto refresh time" - property. Id the value is 0 the automatically updating is disabled. -------------------------------------------
Posted By aOptixUser Mar 03, 2026 12:32:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi @Flareux, I had the same problem in the same scenario. I solved it by registering an event observer that reacts to a UserLogout event and then terminates the current workflow with a method invocation. It's important that the method call isn't implemented on the dialog box itself. Otherwise, ...
Posted By aOptixUser Jan 15, 2026 07:48:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hello Community, I have the following problem: The customer sometimes wants a four-eyes principle (dual acknowledgement) for his alarms. The workflow looks like this, Any employee can acknowledge alarms if they are logged in, but only an employee with a higher user level can confirm ...
Posted By aOptixUser Jan 13, 2026 01:10:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi Shane, First things first, happy new year :D. Sorry to reply so late. I was just about to write the answer, with screenshots of course. I noticed an error in the flow of the methods. Here the problem was that the dialog box was closed and only then the cancel method was executed - ...
Posted By aOptixUser Dec 22, 2025 02:36:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hello everyone I have the following problem: I have to use SignWorflow for the alerting (4-eyes principle), the user who confirms the alarm has to authenticate. I solved the problem like this: The definition of the alarm takes place in the model, from which the instances for the actual alarming are then ...
Posted By aOptixUser Aug 19, 2025 07:28:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi Jennifer, Yesterday I had the same problem. I changed the properties of the bridged network adapter on my VM and restarted it. I'm also only working with one enabled network adapter. Since then, it's been working. I set up the adapter as shown in the picture:------------------------------ ...
Posted By aOptixUser Aug 06, 2025 03:06:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hey, no problem with the delayed response. I've found a workaround in the meantime. I create a data object in the Converters folder and create variables of the required type within it. The variable names are numbered, and I can use the data object as a converter using a formatted dynamic link. ...
Posted By aOptixUser Jul 30, 2025 01:30:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Thank you very much for the quick response. @AutomateSHANE you got it, thats my issue. I tried casting the "MapValueConverterType" into an alias. Unfortunately, that doesn't work. Especially since Intellisense doesn't recognize the variable converter as a "converter type," and I ...
Posted By aOptixUser Jul 29, 2025 08:53:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hello dear community, I hope I'm posting in the right place. If not, please excuse me; this is my first post. I have the following problem: I created a key-value converter (type) in the "Converters" folder and would like to link it to the path property of an image container using a runtime script. ...