List of Contributions

Prasad

Contact Details

Prasad


My Content

1 to 20 of 30 total
Posted By Prasad Mar 10, 2026 09:06:00 AM
Found In Egroup: Advanced Software
\ view thread
Hi Forum, I recently came to know that FactoryTalk AssetCentre does not have a native disaster recovery method for the Micro800 controller family. Has anyone come across a solution for this? I would like to hear your thoughts or approaches on this. -------------------------------------------
Posted By Prasad Mar 29, 2025 12:09:00 AM
Found In Egroup: Advanced Software
\ view thread
below is the pen configuration
Posted By Prasad Mar 28, 2025 04:15:00 AM
Found In Egroup: Advanced Software
\ view thread
hello forum, am trying to print the trend in reports, similar to printing the datalogger, when i click generate PDF the pdf is getting generated, yet only the trend layout is coming not the actual traces of the pen.
Posted By Prasad Dec 09, 2024 06:47:00 AM
Found In Egroup: Advanced Software
\ view thread
Posted By Prasad Dec 09, 2024 06:45:00 AM
Found In Egroup: Advanced Software
\ view thread
Hello forum, am trying to sort the database in the alarm event logger, based on the message value using sql query, but its throwing me syntax error at 49, other than message_en-us column if i try to sort with severity or timestamp its working. If i declare 'message_en-us' as string error is ...
Posted By Prasad Oct 30, 2024 01:42:16 AM
Found In Library: Advanced Software
Posted By Prasad Oct 30, 2024 01:42:00 AM
Found In Egroup: Advanced Software
\ view thread
+++
Posted By Prasad Oct 29, 2024 05:36:00 AM
Found In Egroup: Advanced Software
\ view thread
the syntax is correct
Posted By Prasad Oct 28, 2024 11:09:00 AM
Found In Egroup: Advanced Software
\ view thread
yes am using SetVariableValue. like i said earlier am using the same method and same query to fetch data in datagrid which works fine. what am i missing?
Posted By Prasad Oct 24, 2024 03:43:00 PM
Found In Egroup: Advanced Software
\ view thread
Hello Forum, I'm facing issue while trying to filter the historical trend using SQL Queries. I'm using the same queries for extracting the datalog which is working fine.
Posted By Prasad Aug 29, 2024 12:48:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
The thing is am facing the same issue in 6 drives every time I power up the drive, so i don't think it might be due to faulty control board either.
Posted By Prasad Aug 29, 2024 12:45:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hello forum, am facing an issue with PF755TS every time power cycle is happening am getting F67 [PwrDn Data Fail]. I followed the technote ID: QA64975 i tried checking the wiring, resetting the device and updating the firmware too, as stated in the technote, but the issue is not solved. The last option ...
Posted By Prasad Aug 12, 2024 07:50:00 AM
Found In Egroup: Advanced Software
\ view thread
like am getting two signed int value tag[1] is -26624 and tag[2] is 17837 with the help of COP instruction i set my source as tag[1] and destination tag as real and the converted will be 5555.0, which is the actual displayed value of the scale.
Posted By Prasad Aug 09, 2024 03:00:00 AM
Found In Egroup: Advanced Software
\ view thread
Hello Forum, am using Modbus TCP to read data from weigh scale and getting two int value in two individual tags, that i need to merge to get the actual value(Float) of the weigh scale. I usually do this using PLC with SWPB and COP Instruction. But right now i want to eliminate using a data concentrator. ...
Posted By Prasad Aug 05, 2024 04:40:00 AM
Found In Egroup: Advanced Software
\ view thread
Hi, As you said the values shown in the right column of the editor are the values coming from the field, yes indeed. Here i have used "Model" tags NOT the PLC tags, which i haven't configured in retentivity storage, like you stated, it has to be cleared if panel is rebooted but here it's not happening ...
Posted By Prasad Aug 01, 2024 02:02:03 PM
Found In Library: Advanced Software
Posted By Prasad Aug 01, 2024 02:02:00 PM
Found In Egroup: Advanced Software
\ view thread
Hello Forum, I'm facing an issue in retaining the last applied recipe in "Optix Panel", if I power cycle the panel sometimes it's retaining the selected recipe and sometimes it's not retaining and sometimes it even apply some other recipe after power cycle, Note: In scada based hmi this issue not ...
Posted By Prasad Jul 06, 2024 04:30:00 AM
Found In Egroup: Advanced Software
\ view thread
Hello Forum, am unable to read data from my pf755 using direct connectivity in ft optix, it's throwing me the following error. Might it be due to fw rev?
Posted By Prasad Jul 03, 2024 06:56:00 AM
Found In Egroup: Automation Control
\ view thread
That 8191 value was set as sensor resolution in conversion, so it directly showing there. But it's not the received data. The Base am using is 1734-TOP according to KB ID: IN857 it does state TOP will support 1734-SSI. Verified V+ V- too output does come. EDIT: linkified technote ...
Posted By Prasad Jul 02, 2024 12:53:00 PM
Found In Egroup: Automation Control
\ view thread
Those input are not connected right now, it was earlier wiring diagram.