List of Contributions

Michael Winders

Contact Details

Michael Winders

My Content

1 to 19 of 19 total
Posted By Michael Winders May 13, 2025 12:03:00 PM
Found In Egroup: Automation Control
\ view thread
Hi All My company is looking to improve security across all devices and have asked if I can disable HTTP on the 1756-EN2T cards. It this possible? If not are the new network cards capable of HTTP disabled? This would be a great reason to upgrade all my CPUs and EN2T cards if I can show security ...
Posted By Michael Winders Apr 14, 2025 10:54:00 AM
Found In Egroup: Automation Control
\ view thread
Hi All! I was wondering if Connected components Workbench (CCW) will work with older ArmorStart Drives? Like a 284E or 294E. If CCW can what do I have to load to make them work? Thanks! EDIT: moved to Automation Control community -FL
Posted By Michael Winders Oct 27, 2023 10:42:00 AM
Found In Egroup: Automation Control
\ view thread
As the tech note said - I reinstalled visual C++ and the install worked. ------------------------------ Michael Winders ------------------------------
Posted By Michael Winders Oct 23, 2023 10:20:00 AM
Found In Egroup: Automation Control
\ view thread
Hi All! I am installing Logix 5000 on our new server and am getting this error when I try adding other versions from the file "32.02.01_Studio5000-Multiversion-Web". I realize I can just go find the the C++ distro but I don't remember doing this before. Shouldn't this install without the separate ...
Posted By Michael Winders Oct 23, 2023 10:19:44 AM
Found In Library: Automation Control
Posted By Michael Winders Feb 06, 2023 10:21:00 AM
Found In Egroup: Advanced Software
\ view thread
That triggered my memory - I found that error in the installation guide on page 103 FactoryTalk AssetCentre Installation Guide (rockwellautomation.com) Thanks! ------------------------------ Michael Winders ------------------------------
Posted By Michael Winders Feb 06, 2023 09:32:00 AM
Found In Egroup: Advanced Software
\ view thread
Hi all - I am having a brain fart on how I fixed this before. I don't remember how to update the SSL.YLS cert. ------------------------------ Michael Winders ------------------------------
Posted By Michael Winders Nov 01, 2022 01:38:00 PM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
We ended up reducing the FLA a little more to be within range. ------------------------------ Michael Winders ------------------------------
Posted By Michael Winders Nov 01, 2022 12:42:00 PM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Thanks for the quick response - I missed those parameters. I'll see what I can set to stop the issue. We did put a clam meter on, and the readings are correct. Thanks Again! ------------------------------ Michael Winders ------------------------------
Posted By Michael Winders Nov 01, 2022 10:50:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi All I am looking for a more exact reason for the "Motor current below UL level for more than UL trip delay time." We just replaced the motor and started to get this fault. I lowered the FLA setting, and it seems to help but I am still getting a warning. I am leaning towards the new motor has issues, ...
Posted By Michael Winders Jun 23, 2022 09:57:00 AM
Found In Egroup: Legacy
\ view thread
Hi All I am looking at setting the SNMP password on a 1747-L552/C SLC-5/05 CPU. I am using the GetIf app to try and set it like with out L73 PLCs but I am not seeing the parameter. I do see SNMP section in the GetIf tree but nothing is there for the read/writ settings. Is this even possible with the ...
Posted By Michael Winders Mar 08, 2022 01:47:00 PM
Found In Egroup: Automation Control
\ view thread
Hmm - I am not sure if CIP limits are the same a Modbus. Maybe use a separate ProSoft module EthernetIP to Modbus485 (Or equivilant)? Then the 870 will be talking to one device (Server) at that point. ------------------------------ Michael Winders ------------------------------
Posted By Michael Winders Mar 08, 2022 10:24:00 AM
Found In Egroup: Automation Control
\ view thread
I believe so - As long as all the devices have different Modbus addresses configured. 254 is the max number if I remember correctly. ------------------------------ Michael Winders ------------------------------
Posted By Michael Winders Mar 03, 2022 11:17:00 AM
Found In Egroup: Advanced Software
\ view thread
We changed the temp file directory to not be read-only and ran the schedule again, this resolved the issue. The directory was at C:\ProgramData\Rockwell\AssetCentre\DisasterRecoveryTempFiles\ProductionFiles. The other thing is after the change the directory went back to read-only but continues ...
Posted By Michael Winders Feb 21, 2022 02:55:00 PM
Found In Egroup: Advanced Software
\ view thread
Any other possible issues? ------------------------------ Michael Winders ------------------------------
Posted By Michael Winders Feb 17, 2022 09:50:00 AM
Found In Egroup: Advanced Software
\ view thread
The permissions and logs all look good... (I think?) I also have a ticket open on this 4009475008 or 211020-008599 ------------------------------ Michael Winders ------------------------------
Posted By Michael Winders Feb 17, 2022 09:28:00 AM
Found In Egroup: Advanced Software
\ view thread
Hi Austin I am on the same Server and I don't have any agents yet (I think - I am a newbe at FT Asset Centre) ------------------------------ Michael Winders ------------------------------
Posted By Michael Winders Feb 16, 2022 03:53:00 PM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
I found this in the documentation - I am not sure if it will help... ------------------------------ Michael Winders ------------------------------
Posted By Michael Winders Feb 16, 2022 01:39:00 PM
Found In Egroup: Advanced Software
\ view thread
I am getting these errors in my logs... How do I fix this? Thanks! ------------------------------ Michael Winders ------------------------------