List of Contributions

Malike

Contact Details

Malike

My Content

1 to 3 of 3 total
Posted By Malike Apr 22, 2026 02:35:00 AM
Found In Egroup: Advanced Software
\ view thread
Hi @Philip Hamilton, I have tried the suggestions, but the issue still persists. As an alternative, I installed a fresh instance of Windows Server 2022 for runtime client testing. When the system is run from a client using Windows Server 2022, it operates correctly, as the same applies on Windows 11. ...
Posted By Malike Apr 19, 2026 11:54:00 PM
Found In Egroup: Advanced Software
\ view thread
My project is "Distributed Application" using FT SE version 16 in Windows Server 2022 and for client computer is Windows 11. I got some problem with the client computer, when i test the display using play button in FT SE server studio or using runtime client in Server computer, the nametag is still normal. ...
Posted By Malike Jul 10, 2025 02:06:00 AM
Found In Egroup: Advanced Software
\ view thread
I have a question about redundant FTLinx in FTView SE Server system. The case, there is 2 server computers that have 2 different LAN connections each, #1=connection PC/HMI (used for connection to FTDS and another client) and #2=connection PLC. The issue is, when the LAN connection #1 PC/HMI is problem/off ...