List of Contributions

Loganathan

Contact Details

Loganathan

My Content

1 to 20 of 27 total
Posted By Loganathan Jan 06, 2026 07:10:05 AM
Found In Egroup: Emulate3D Software
\ view thread
Hi Team, Is there any catalog items that would help in emulating Nutrunners? Any help would be greatly appreciated. Thanks Thilak Loganathan -------------------------------------------
Posted By Loganathan Dec 26, 2025 12:09:16 PM
Found In Egroup: Emulate3D Software
\ view thread
Hi Cannon, Thanks for your response. Without parenting the part to the skid, how to create both the loads at the same time? is there any way to that? Can you share the additional information on the custom gripper controller that you use. That would be very good to take it forward. ------------ ...
Posted By Loganathan Dec 23, 2025 01:53:00 PM
Found In Egroup: Emulate3D Software
\ view thread
The skid, along with the part, moves on a conveyor controlled by a VFD. Skid is the parent and part is the child. When the skid is blocked by a sensor, the skid stops, and the robot needs to pick up the part. The robot should pick only the part, while the skid moves empty to the next station. The robot ...
Posted By Loganathan Dec 17, 2025 03:32:00 PM
Found In Egroup: Emulate3D Software
\ view thread
I have mapped all the tags from the PLC connected to a specific IP address. However, when I connect to another PLC with different IP address, all the mapped tags are lost, and I need to add them again. Is there a way to retain the tag mapping after changing the IP address? ------------------------- ...
Posted By Loganathan Dec 17, 2025 03:27:00 PM
Found In Egroup: Emulate3D Software
\ view thread
I need to establish a Class 1 connection for the end-of-arm tools to write tags to the PLC, but I am only getting a Class 3 connection. For HMIs, safety blocks, and light screens, I was able to establish a Class 1 connection. -------------------------------------------
Posted By Loganathan Dec 04, 2025 09:33:00 AM
Found In Egroup: Emulate3D Software
\ view thread
We are emulating a tire and wheel station where a vehicle moves along a skid on a conveyor, and tires are placed by robots. Both the vehicle and the tires are treated as loads. When the robot installs the wheel onto the vehicle, after the process is completed, the tire needs to move together with the ...
Posted By Loganathan Nov 21, 2025 11:32:00 AM
Found In Egroup: Emulate3D Software
\ view thread
We are in need of the Armor PowerFlex 35S, and we've heard from the E3D team that a beta version is available. Could you please let us know when we can expect an update on this? This is currently holding us back from completing the project, so any assistance would be greatly appreciated. Thank you, Thilak ...
Posted By Loganathan Nov 18, 2025 09:15:05 AM
Found In Egroup: Emulate3D Software
\ view thread
Thank you for your response. I am currently using the Controlled Load Creator from the Load Creator Catalog. I have mapped the Create Load property to an address. However, whenever I attempt to create the load using the tag, the Kinematic property in the rigid body becomes unchecked, causing the load ...
Posted By Loganathan Nov 18, 2025 09:14:50 AM
Found In Egroup: Emulate3D Software
\ view thread
Thank you for your response. I am currently using the Controlled Load Creator from the Load Creator Catalog. I have mapped the Create Load property to an address. However, whenever I attempt to create the load using the tag, the Kinematic property in the rigid body becomes unchecked, causing the load ...
Posted By Loganathan Nov 13, 2025 12:57:00 PM
Found In Egroup: Emulate3D Software
\ view thread
We are controlling robots through Roboguide and emulating them using a PLC. We have defined physics for the gripper and other properties in Aspect Viewer. The robot is successfully picking and dropping the part. However, when the robot starts the next cycle, we need the existing loads to be deleted and ...
Posted By Loganathan Oct 28, 2025 09:17:52 AM
Found In Egroup: Emulate3D Software
\ view thread
Hi Pascal, Yes. We generated safety signature and locked safety. The reason for that is to clear the safety signature faults on the HMI. -------------------------------------------
Posted By Loganathan Oct 27, 2025 03:36:00 PM
Found In Egroup: Emulate3D Software
\ view thread
Can someone help me with solving this error. It was working fine and without making any changes to the PLC, i am getting this error Thanks in advance Thilak Loganathan -------------------------------------------
Posted By Loganathan Jul 11, 2025 07:41:00 AM
Found In Egroup: Emulate3D Software
\ view thread
Hi Andy, That's Awesome. Thanks a lot. Will check this out and come back to you. Regards Thilak Loganathan
Posted By Loganathan Jul 10, 2025 03:07:00 PM
Found In Egroup: Emulate3D Software
\ view thread
Hi Andy, Great to hear about your emulator for the Armor Power Flex! Our application is for an automotive project. We're in the early stages and could definitely benefit from a head start. Any help would be great. Thanks, Thilak
Posted By Loganathan Jul 10, 2025 10:51:00 AM
Found In Egroup: Emulate3D Software
\ view thread
Hi Deebs, Thanks for your response and glad to know that. Also, Is there any timeline on when we expect? We are stuck on this in our current project and if we have a timeline then it would be great. Regards Thilak
Posted By Loganathan Jul 08, 2025 03:03:00 PM
Found In Egroup: Emulate3D Software
\ view thread
Hello, Currently we don't have an ArmorPowerFlex VFD in the emulate 3D catalog. Is there any possibility to add that into the catalog or Is there a way to emulate it using any of the other VFD's that is there in the catalog already? Any support would be greatly appreciated Thanks Thilak L ...
Posted By Loganathan May 14, 2025 10:49:00 AM
Found In Egroup: Emulate3D Software
\ view thread
Hello Team, I am encountering the following errors when installing the Prox sensor from the catalog. Can you please help me with this? Thanks Thilak Loganathan
Posted By Loganathan May 09, 2025 08:09:00 AM
Found In Egroup: Emulate3D Software
\ view thread
Hi Mike, Thank you for your prompt response. I have followed the method you provided: It works well on the conveyors from the catalog. However, there is an offset issue with the CiTM powered conveyors. I've attached an image for your reference. Could you please assist with this? Best ...
Posted By Loganathan May 08, 2025 03:19:20 PM
Found In Library: Emulate3D Software
Posted By Loganathan May 08, 2025 03:19:00 PM
Found In Egroup: Emulate3D Software
\ view thread
Hi Mike, Thanks for the video. It was helpful. Also, I encountered another issue. I have my own skid& part models for which I added the load property via the Aspect Viewer and the conveyor property for the conveyor. However, when I create the loads using the Load Creator, there is an offset. ...