List of Contributions

Ryan Murphy

Contact Details

Ryan Murphy

My Content

1 to 20 of 50+ total
Posted By Ryan Murphy Jan 13, 2026 03:03:00 PM
Found In Egroup: General Discussions
\ view thread
Cleared all cookies, and cache and it seems to work in chrome now. I guess something went stale? ------------------------------ Regards, RM ------------------------------
Posted By Ryan Murphy Jan 13, 2026 02:54:00 PM
Found In Egroup: Installation & Activation
\ view thread
I can apparently no longer download from the PCDC. Stuck in a forever loop of Download Now -> Redirect to Login -> Downloads -> Download Now -> Redirect to Login. I am using Chrome, still. Cookies are enabled, still. Why do you have to make things so difficult? After being stuck in the same loop ...
Posted By Ryan Murphy Dec 02, 2025 01:51:13 PM
Found In Egroup: Automation Control
\ view thread
Sorry to butt in, but I wanted some clarification: Is FT Design Workbench replacing CCW? Is it just a rebrand of CCW? Had not heard of FT Design Workbench until reading this post, but then I also have never actually worked with the Micro800 controllers. ------------------------------ Regards, RM ...
Posted By Ryan Murphy Nov 19, 2025 09:18:00 AM
Found In Egroup: Networks
\ view thread
Alright, this is an issue that pops up on different machines from time to time. Have seen it on Stratix 5700 and 5200. We do short press Express Setup and often leave it at that, but intermittently I get a fault from the switch (switch alarm relay wired to Point I/O or Flex 5000 Input). When I look in ...
Posted By Ryan Murphy Nov 19, 2025 09:05:36 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
In addition to Josh Hewitt's suggestion about the axis feedback configuration, I was also wondering whether you have your PLC loading from non-volatile memory on power-up and possibly overwriting the AxisHomedStatus. That was the gist of my question regarding PLC also powering down or just drives powering ...
Posted By Ryan Murphy Nov 18, 2025 09:22:50 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi, So when you power the rack up again the AxisHomedStatus bit is low? The APRFault bit is high? Is this with only the servo rack powering down or is the PLC also being powered down? I am assuming Controllogix? What are the firmware versions of the Drive and of the PLC? I would not think changing ...
Posted By Ryan Murphy Nov 17, 2025 02:47:13 PM
Found In Egroup: Automation Control
\ view thread
Have not seen the issue since forcing the port configuration of the EN2T to 100/Full. I guess that fixed it? Now that I have said that I fully expect it to come back within the next hour. Or fifteen minutes after I leave the machine tonight. ------------------------------ Regards, RM ----------- ...
Posted By Ryan Murphy Nov 17, 2025 02:41:36 PM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Maybe I am being unintentionally obtuse, but isn't 49 just the drive powerup marker? Not really a fault per-se, just a message in the queue indicating power was cycled. Page 319 of the programming manual found here: https://literature.rockwellautomation.com/idc/groups/literature/documents/pm/750 ...
Posted By Ryan Murphy Nov 13, 2025 08:42:44 AM
Found In Egroup: General Discussions
\ view thread
Detroit, Michigan area here. ------------------------------ Regards, RM ------------------------------
Posted By Ryan Murphy Nov 07, 2025 09:17:41 AM
Found In Egroup: Automation Control
\ view thread
More information, sorry for not including some of this in the original post: Enet port on cpu is not used. Going through a EN2T v11.002 (config as 11.001, compatible). Connection occurs through a Stratix 5200 (CMS10DN) switch. Express setup has been performed on the switch, but little else was done ...
Posted By Ryan Murphy Nov 06, 2025 03:31:00 PM
Found In Egroup: Automation Control
\ view thread
I have a 5094-IB16S with an E-Stop wired to points 0 and 1. Intermittently, as far as I can tell, one or both of the status bits drops out which causes the DCI instruction in safety to fault. The fault on the instruction when this happens is: So far I have noticed it happen 2-3 times per day ...
Posted By Ryan Murphy Oct 24, 2025 09:26:37 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Are the motors coupled to load or are they free and showing the 5% and 35% current draw? One of the quickest sanity checks for me usually is to decouple from the load. Then when I figure out it was something stupid I did I just tell the builder that the coupler must not have been straight. :-P --- ...
Posted By Ryan Murphy Sep 11, 2025 11:20:48 AM
Found In Egroup: Automation Control
\ view thread
Hi Lin, Take a look at this (sorry, TC locked): ID: QA29347 | Access Levels: TechConnect How to Implement HORM on the MobileView Terminal ------------------------------ Regards, RM ------------------------------
Posted By Ryan Murphy Sep 11, 2025 11:13:00 AM
Found In Egroup: Automation Control
\ view thread
Unfortunately that is the only way I know of to know which file is currently running. I hate when multiple mers pile up on a panelview for this very reason. ------------------------------ Regards, RM ------------------------------
Posted By Ryan Murphy Sep 11, 2025 10:37:19 AM
Found In Egroup: General Discussions
\ view thread
"Also on a different subject: OPTIX needs its own channel, wowee has that thing blown up... and you need to put @AutomateSHANE on the payroll. " Emulate3D also has blown up. I don't often look beyond the home page so may be missing some non-Optix and Emulate3D posts. I am not even in the Emulate 3D ...
Posted By Ryan Murphy Sep 10, 2025 01:20:41 PM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hi Dave, C122 cannot be programatically changed. See: ID: QA39792 | Access Levels: Everyone PowerFlex 525: Parameter C122 [Cmd Stat Select] will not change However, could you not set yourself up for Position Control and then use the Jog function for times when you need to switch to speed control? ...
Posted By Ryan Murphy Sep 08, 2025 01:38:13 PM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
I did not realize it, but seemingly there is a Profinet adapter for the PF525: https://literature.rockwellautomation.com/idc/groups/literature/documents/um/520com-um005_-en-p.pdf Might simplify your life if the manual that Fuzzy pointed you to doesn't work for you. ------------------------------ ...
Posted By Ryan Murphy Sep 02, 2025 02:55:00 PM
Found In Egroup: Automation Control
\ view thread
I believe the short answer to your question is "No." ID: IN40175 | Access Levels: Everyone PanelView 800 firmware v8.011 and hardware series changes Supposedly MicroLogix1400 is still supported, it appears, but nothing else in the RSLogix500 series of processors. ------------------------------ ...
Posted By Ryan Murphy Aug 18, 2025 12:20:09 PM
Found In Egroup: Advanced Software
\ view thread
Instead of an AOI you could put the logic in a routine and JSR to it, passing values to it? Then the string inside the UDT is accessible. ------------------------------ Regards, RM ------------------------------
Posted By Ryan Murphy Aug 15, 2025 01:46:00 PM
Found In Egroup: Advanced Software
\ view thread
Not that I know of. Anything other than an Atomic data type (SINT, DINT, INT, REAL, BOOL) can only be passed by reference (InOut Parameter). EDIT: I suppose a really terrible workaround would be to pass each character as a SINT. ------------------------------ Regards, RM ---------------------- ...