List of Contributions

Galayda

Contact Details

Galayda

My Content

1 to 19 of 19 total
Posted By Galayda Sep 30, 2025 09:46:39 PM
Found In Egroup: Automation Control
\ view thread
There is another option, add a 1:1 transformer, AKA line reactor, to your PS input. That way, the Power supply will be decoupled from the GFCI -------------------------------------------
Posted By Galayda Sep 29, 2025 01:42:00 PM
Found In Egroup: Automation Control
\ view thread
I was there about a month ago. Had a new power supply installed by the plant's maintenance team. Think they got it from Radwell or something. Didn't solve a problem. New GFCIs, a wall outlet type and household panel mounted once, are super sensitive and don't like capacitive loads with low switching ...
Posted By Galayda Jun 27, 2025 08:14:00 PM
Found In Egroup: Automation Control
\ view thread
Local variables are calculated by your code. What does your program do? I feel like something is writing wrong data types in to name0, 1 and 2. If you want to flip output change them in global variables.
Posted By Galayda Jun 25, 2025 06:00:00 PM
Found In Egroup: Automation Control
\ view thread
Does it stay slow? I have designed few systems at work with 2080-LC50 and 2711R. I found every single time on boot all elements are slow to respond until you change the screen or interact with the element. Trying to use buttons or numerical fields again and they react much faster. Regarding validation ...
Posted By Galayda Jun 25, 2025 02:41:00 PM
Found In Egroup: Automation Control
\ view thread
I also had to copy file mentioned in update 4 for 48qbb, otherwise it was failing update
Posted By Galayda Jun 25, 2025 12:07:00 AM
Found In Egroup: Automation Control
\ view thread
OK, I think i have figured it out. At least I did recover my 48QBB. I was using ControlFlash for recovery. First you will need to locate folder with firmware files. In my case it was C:\Program Files (x86)\ControlFLASH\0001\000E. There are multiple subfolders corresponding to different controllers, ...
Posted By Galayda Jun 24, 2025 09:57:00 PM
Found In Egroup: Automation Control
\ view thread
Have anyone experienced something like this? Absolutely. I have 7 controllers sitting on my desk right now with failed flash. Solution? I haven't found one yet. What did you use to flash controllers? Control Flash or Plus version? Did you flash using USB, serial or Ethernet? What is the manufacturing ...
Posted By Galayda Jun 19, 2025 01:20:00 AM
Found In Egroup: Automation Control
\ view thread
Hey everyone. I have a few micro 850 controllers that failed firmware update. AWBs, QWBs and QBBs in both 24 and 48 port flavors. Every single one only could be visible trough virtual backplane and report to be 2080-LC50. Control Flash generates a log with ERROR #2100: Catalog registry validation error ...
Posted By Galayda Jan 31, 2025 11:53:00 AM
Found In Egroup: Automation Control
\ view thread
How are you reading 6 flow meters at the same time? Ladder logic with 6 blocks for MSG_Modbus? Or you doing ST? if its a ladder logic, just put 6 blocks on the same rung so one doesn't execute until previous one .Q is true
Posted By Galayda Jan 31, 2025 02:58:00 AM
Found In Egroup: Automation Control
\ view thread
What do you mean by communicating with all six simultaneously? Do you try to send or receive data from 6 devices simultaneously? I don't think it works that way for serial data communication. What I have done in the past is have had a function block that had "done" output when a message is sent or received, ...
Posted By Galayda Jan 08, 2025 02:09:00 AM
Found In Egroup: Automation Control
\ view thread
You should be able to do implicit messaging using 2080-L50E and it's relatively easy to setup using example linked by nmeistrup. If you are using LC50, modbus is your friend as it doesn't support explicit messaging.
Posted By Galayda Jan 03, 2025 09:49:00 PM
Found In Egroup: Automation Control
\ view thread
I just finished wiping and reinstalling Windows on my Dell XPS. I installed freshly downloaded CCW, and it won't validate. So far, all my AMD machines work fine on 24H2, and none of the Intel-powered ones pass validation. Sadly, if you download a fresh copy of Windows, 24H2 is baked in already. Also, ...
Posted By Galayda Jan 03, 2025 02:17:00 PM
Found In Egroup: Automation Control
\ view thread
A diagram and make model of the actuator would help a lot. Are you using electromechanical relays for PWM drive of DC motors? I would use SCRs to prevent contact chatter; even at 4 amps with constant switching, relay contacts will arc just enough to wear out rather quickly. You can control the direction ...
Posted By Galayda Dec 31, 2024 12:25:00 PM
Found In Egroup: Automation Control
\ view thread
This is interesting, because I installed CCW on my desktop running windows 11 and it worked fine. Installed 24H2, as I suspected it might be an issue, and it works fine. Have 2 desktops and 2 laptops with 24H2 and only one laptop not working.
Posted By Galayda Dec 29, 2024 01:04:00 AM
Found In Egroup: Automation Control
\ view thread
I also tried fixing, uninstalling/installing C++ 2013 and Visual Studio 2015 Shell, but no changes.
Posted By Galayda Dec 28, 2024 08:53:00 PM
Found In Egroup: Automation Control
\ view thread
Tried uninstalling everything that has Rockwell on it, removed Rockwell automation and Rockwell software from %appdata% did the same thing with registry in \HKEY_LOCAL_MACHINE\SOFTWARE and \HKEY_CURRENT_USER\Software. This time, I got a prompt to pick a network adapter, but the application still didn't ...
Posted By Galayda Dec 26, 2024 12:53:00 PM
Found In Egroup: Automation Control
\ view thread
I thought 24H2 might be an issue, but it works fine on my other computer after 24H2 installation. I tried a full purge of everything Rockwell followed with registry cleaning, but it didn't work. One thing I have noticed is some files were left somewhere. During re-installation, I didn't get a prompt ...
Posted By Galayda Dec 23, 2024 06:30:00 PM
Found In Egroup: Automation Control
\ view thread
Standard edition CCW 22.0, Opened project created in, I belive CCW 13. CCW automatically updated all database files. Saved a project under a different name, and HMI validated just fine. I didn't try adding new tags to the project. I had an error compiling for 850 as well, when changing controller type. ...
Posted By Galayda Dec 22, 2024 03:19:00 AM
Found In Egroup: Automation Control
\ view thread
I just found myself in the same boat. Made custom UDFB to work with HMI. Working with 2711R-T7T would not validate the application at all. I got it down to one push button and one tag attached to it, and it wouldn't go. Opening previous projects from a few years ago validates just fine. I saved the project ...