Skip to main content (Press Enter).
Sign in
Skip auxiliary navigation (Press Enter).
Rockwell Automation
Contact Us
Terms and Conditions
Skip main navigation (Press Enter).
Toggle navigation
Home
Member Directory
Profile
My Contributions
List of Contributions
List of Contributions
STEVE BINKS
Contact Details
×
Enter Password
Enter Password
Confirm Password
STEVE BINKS
Profile
Connections
Contacts
Contributions
Summary
Achievements
List of Contributions
My Content
1 to 20 of 24 total
search criteria =
ALL
Logix5000 V13 activation
Posted By
STEVE BINKS
Mar 10, 2025 03:39:00 AM
Found In
Egroup:
Installation & Activation
\
view thread
I have 2 W10 VMs, a network one which can load V13 programs, and a local one which tries to run EVmove (and failing because its not a 64 bit program). Both machines have the same licenses, a legacy one which I understand uses Flexera not codemeter Use CodeMeter First checkbox is cleared ...
RE: How to read capacity in 5580 controller
Posted By
STEVE BINKS
Jan 31, 2025 08:38:00 AM
Found In
Egroup:
Automation Control
\
view thread
There is a processor HMI faceplate available in sample code
RE: Panelview shows Channel underrange when channel alarms are disabled
Posted By
STEVE BINKS
Jan 31, 2025 08:27:00 AM
Found In
Egroup:
Automation Control
\
view thread
Try Unlatching the channel Underrange bit every scan
RE: 5069-SERIAL (on a 5380) throws a 16#001e when executing a MSG
Posted By
STEVE BINKS
Jan 23, 2025 05:59:00 AM
Found In
Egroup:
Automation Control
\
view thread
Is there, maybe, a master reset that can be done on the processor without turning it into a brick? Yes there is a small hole under the run switch where you can insert a paperclip while powering up, this clears the memory - useful on a safety PLC when you can't remember the password ;0
RE: 1756-L61 Ser B FW 1.1 update firmware issue...
Posted By
STEVE BINKS
Dec 05, 2024 06:23:00 AM
Found In
Egroup:
Automation Control
\
view thread
FW v1.1 is a virgin device, previously unused SO flash it in a bench setup as above, if you can use a Ethernet card like EN2T with a USB port then use that
RE: L83E Embedded Ethernet Port
Posted By
STEVE BINKS
Dec 02, 2024 07:58:00 AM
Found In
Egroup:
Automation Control
\
view thread
Put the other PLC in each others IO tree at the bottom, with their IP addresses, then configure your produced tags with 1 consumer, then your consumed tags with the producer selected from the IO tree, make sure both PLC are set to same task rates. are you sending safety tags?
RE: L61 v20 - Should I be able to import a datatype Online?
Posted By
STEVE BINKS
Dec 02, 2024 07:47:00 AM
Found In
Egroup:
Automation Control
\
view thread
I can hear tech support saying " have you installed the latest version?" I have done this on 20.05 but NOT online Steve
RE: 1734-FPD function
Posted By
STEVE BINKS
Dec 02, 2024 07:41:00 AM
Found In
Egroup:
Automation Control
\
view thread
Your FPD likely provides Emergency stopped power to the output cards so that all points on those cards will be off for an E-stop. So you should put your input card before the FPD and re-map the 2 output cards Steve
RE: PvP 7 plus print button
Posted By
STEVE BINKS
Dec 02, 2024 07:37:00 AM
Found In
Egroup:
Automation Control
\
view thread
In Global Connections - Display, you can find the Remote Display Number to display the chart object page, then Remote Display Print to print the page on view Steve
Failed to instatiate Module profile, The sever was faulted by a previous call
Posted By
STEVE BINKS
Dec 02, 2024 01:02:00 AM
Found In
Egroup:
Automation Control
\
view thread
Logix v33 on W10, added EDS files for multiple PLX32-EIP modbus cards, now when selecting my card I get error 8612-80043A12 Rebooting makes no difference, help file is no help, Knowledgebase seems to have no entry for this error Does anyone have any tips Steve
RE: PF40 upgrade to PF525, reading parameter
Posted By
STEVE BINKS
Nov 07, 2024 07:24:00 AM
Found In
Egroup:
Drives, Motion Control & Low Voltage Products
\
view thread
Hi Ryan I would normally do that for reading current or power, that change all the time, but not for a value that should be constant. Which is why I followed the original messaging technique, it only talks to each inverter once every 12 seconds instead of very 200ms Is there ...
RE: Had to downgrade FW on 755 - how to easily change the Device in IO tree as well
Posted By
STEVE BINKS
Nov 07, 2024 04:37:00 AM
Found In
Egroup:
Drives, Motion Control & Low Voltage Products
\
view thread
Note to self, keep old AOP downloads
PF40 upgrade to PF525, reading parameter
Posted By
STEVE BINKS
Nov 07, 2024 04:30:00 AM
Found In
Egroup:
Drives, Motion Control & Low Voltage Products
\
view thread
Hi All, upgrading several (12) PF40 to PF525, trying to re-use the parameter read message for Max Speed but failing with error 16#0001 ext code 16#0001_0315, obviously changed the parameter field to 44. In communication tab I see the correct drive name passed in from an array e.g. $01$02$12$p192.168.2.15 ...
PF525 C-P MISMATCH
Posted By
STEVE BINKS
Mar 20, 2024 02:12:00 AM
Found In
Egroup:
Drives, Motion Control & Low Voltage Products
\
view thread
I have a PF525 7.5HP 5.5KW 460V which thinks its a 460V 1.0HP After setting par#53 to 3 (Power Reset) its still the same After flashing v7.001 ( which it originally came with) it thinks it is 600V 2.0HP After setting par#53 to 3 (Power Reset) its back to 460V 1.0HP Is there anything ...
RE: Error 716-80042001 "Failed to create project file...Couldn't be found."
Posted By
STEVE BINKS
Jan 29, 2024 03:25:00 AM
Found In
Egroup:
Automation Control
\
view thread
Hi Sarille This is a massive problem for lots of us, Studio5000 loses a temporary file it created and I wish Rockwell could get to the bottom of it Registry tuning, viruses, UAC (User Access Control) and various other reasons have been blamed It has even been suggested that I uninstall ...
RE: Powerflex rpm and poles parameters
Posted By
STEVE BINKS
Jan 18, 2024 09:33:00 AM
Found In
Egroup:
Drives, Motion Control & Low Voltage Products
\
view thread
And if I cannot access the motor rating plate so don't know poles or rpm, what effect will this have on the motor e.g use the default 2 poles for a 4 poles motor ------------------------------ STEVE BINKS ------------------------------
Powerflex rpm and poles parameters
Posted By
STEVE BINKS
Jan 17, 2024 08:27:00 AM
Found In
Egroup:
Drives, Motion Control & Low Voltage Products
\
view thread
I have a motor that is unreachable without the scaffolding that it was installed with, so unsure of exact details on rating plate. Do the rpm and number of poles parameters do anything critical other than provide rpm readout? PF525 but also PF753/755 for future reference ------------------------------ ...
RE: PF755 STO over ethernet
Posted By
STEVE BINKS
Dec 19, 2023 06:06:00 AM
Found In
Egroup:
Drives, Motion Control & Low Voltage Products
\
view thread
Hi Mica Thanks for the link, but damn Rockwell knows how to charge, that card is 3x the price of the standard STO card so that totally negates the saving of 2 safety outputs So unless its the only drive in the cabinet and I can save on AENT card too, then its not a great saving After working ...
PF755 STO over ethernet
Posted By
STEVE BINKS
Dec 15, 2023 04:21:00 AM
Found In
Egroup:
Drives, Motion Control & Low Voltage Products
\
view thread
I noticed that PF755 EENET can have safety messages, does this mean we can do STO over ethernet, like PF527 If so, its about time, if not, whats taking so long?..... ------------------------------ STEVE BINKS ------------------------------
RE: PowerFlex 525 - Parameter 105 and STO function
Posted By
STEVE BINKS
Dec 15, 2023 04:11:00 AM
Found In
Egroup:
Drives, Motion Control & Low Voltage Products
\
view thread
It only disables the fault F059, so is therefore desirable when using STO ------------------------------ STEVE BINKS ------------------------------
«
1
2
»
Membership
Join the Rockwell Community
Contact
Contact Rockwell Automation
About Us
Copyright 2021. All rights reserved.
Site Design by
eConverse Media
.
Powered by Higher Logic