List of Contributions

Omer Faruk Piskin

Contact Details

Omer Faruk Piskin

My Content

1 to 10 of 10 total
Posted By Omer Faruk Piskin Sep 08, 2025 08:03:25 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
I couldn't figure out what value to enter for the assembly instance. -------------------------------------------
Posted By Omer Faruk Piskin Sep 08, 2025 05:57:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
I would like to communicate an S7-1500 PLC with a PowerFlex 525 drive, but I need the following information. Could you please assist me? -------------------------------------------
Posted By Omer Faruk Piskin Sep 04, 2025 01:38:00 AM
Found In Egroup: Advanced Software
\ view thread
Is it possible in Optix to convert batch files and alarms into PDF and send them to the SCADA system? -------------------------------------------
Posted By Omer Faruk Piskin Sep 02, 2025 01:13:00 AM
Found In Egroup: Automation Control
\ view thread
The 5069 CompactLogix PLC operates with the IP address 192.168.1.111, but after a few weeks it switches to a dynamic IP. The program backup is not deleted; only the IP address changes. What could be the reason for this? -------------------------------------------
Posted By Omer Faruk Piskin Jun 19, 2025 07:05:00 AM
Found In Egroup: Advanced Software
\ view thread
Hello, When I open the Alarm History to view past alarms on the Optix panel, the same alarm appears multiple times in separate rows. I would like each alarm to appear only once, based on the time it occurred. Could you please help me with this?
Posted By Omer Faruk Piskin Mar 21, 2025 08:43:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
In the PowerFlex DC drive, when Parameter 241 (Torque Mode Select) is set to Torque Reg, the system operates without any issues. However, when switched to Speed Reg mode, an F4 (AC Undervoltage) fault occurs. The input voltage has been measured at 400V. Despite setting Parameter 470 to 30 ms, the fault ...
Posted By Omer Faruk Piskin Dec 11, 2024 06:46:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hello, I am driving a servo motor based on feedback from an encoder linked to the load. When the servo motor experiences a delay, it accelerates excessively to compensate for the gap and enters a speed error state Best regards
Posted By Omer Faruk Piskin Dec 11, 2024 12:10:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
I am using the Kinetix 5100 servo drive for Full Closed-loop Control, but when the motor corrects itself based on feedback from the encoder, it accelerates excessively and triggers a fault. Is there a way to limit this correction speed? I tried using parameter P1.076 to restrict it, but it didn't wo ...
Posted By Omer Faruk Piskin Jan 10, 2023 12:35:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
I'm sorry for my late reply. Thank you for your answer. ------------------------------ Omer Faruk Piskin ------------------------------
Posted By Omer Faruk Piskin Jan 04, 2023 06:27:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Can you give information about the use of 'Replace and restart' and 'Replace and continue' in the Cam Type section of the MAPC block? ------------------------------ Omer Faruk Piskin ------------------------------