List of Contributions

TylerK

Contact Details

TylerK

My Content

1 to 8 of 8 total
Posted By TylerK Dec 15, 2025 12:13:16 PM
Found In Egroup: Emulate3D Software
\ view thread
Sorry, there's a COP function in there as well. I can send screenshots if this is still the best way of doing things -------------------------------------------
Posted By TylerK Dec 15, 2025 12:11:23 PM
Found In Egroup: Emulate3D Software
\ view thread
I'm unsure if there's a newer way to do it, but if your cell has CIP safety you'll have to spoof it since currently FANUC ROBOGUIDE doesn't support CIP safety. Regardless, the way I've been doing it over the last few years is to create an emulation subroutine and create a timer and a MSG to get the ...
Posted By TylerK Dec 12, 2025 06:31:30 AM
Found In Egroup: Emulate3D Software
\ view thread
Attempting to build out a cell that uses paint robots. We're using FANUC ROBOGUIDE PaintPRO, and running into problems with making a PLC connection. From my understanding, PaintPRO has a built in PLC-type system for testing, and I can assume that this will create problems. Does anybody have any ...
Posted By TylerK Nov 21, 2025 12:56:37 PM
Found In Egroup: Emulate3D Software
\ view thread
Ah, I apologize. You were correct, this has fixed the issue. I am experiencing a code 8004f207 trying to put one of the modules in from what was on the EN2T but that's a separate issue I'll work through. Thanks for all the help and patience! -------------------------------------------
Posted By TylerK Nov 21, 2025 10:56:21 AM
Found In Egroup: Emulate3D Software
\ view thread
If I move all of the devices under the controller vs the EN2T, I will still be unable to go online via FT Logix Echo unless I use the 127.0.0.1. -------------------------------------------
Posted By TylerK Nov 21, 2025 10:11:02 AM
Found In Egroup: Emulate3D Software
\ view thread
The way I had approached it was similar to having a real switch + PLC + EN2T setup on my second ethernet card. Set the PC/card as its own IP, and everything else is different as to not create IP conflicts. I changed my adapter settings for my loopback network to be the same as the PLC IP in FT Echo ...
Posted By TylerK Nov 21, 2025 07:41:54 AM
Found In Egroup: Emulate3D Software
\ view thread
Mark, So I added the Hyper V adapter and can ping it at 192.168.1.3, and my PC is properly routing 192.168.1 addresses through that adapter, but putting a Logix Echo PLC on that network won't connect. Going off of the "Logix Echo with Loopback Adapter" link you shared, I installed the Windows Loopback ...
Posted By TylerK Nov 20, 2025 02:10:00 PM
Found In Egroup: Emulate3D Software
\ view thread
I had to let go of my switch for another project going on and am currently trying to make do with Logix Echo. I'm able to connect to the Logix Echo Chassis via loopback address, 127.0.0.1, but I know that you cannot make a Class 1 connection via loopback. I'm attempting to connect the PLC to Logix Echo ...