List of Contributions

Retzlaff

Contact Details

Retzlaff

My Content

1 to 20 of 50+ total
Posted By Retzlaff Jan 14, 2026 01:36:53 PM
Found In Egroup: Automation Control
\ view thread
Alright maybe I am missing something here. I wrote some logic for OEE first in Ladder and was using a RTO to accumulate downtime. All worked as expected and in testing phase I can change the .ACC value. In initial testing I found of course problems with the math errors of dividing by zero. So, I rewrote ...
Posted By Retzlaff Jan 07, 2026 04:07:00 PM
Found In Egroup: Advanced Software
\ view thread
I am trying to change the color of a box based on a value of a tag. For instance, anything from 0 - 49 would be red, anything 50 -84 yellow, and anything 85 or above green. I tried a key value converter but can't seem to put expressions in it. Maybe I am doing something wrong but wanted to ask first. ...
Posted By Retzlaff Jan 02, 2026 10:17:00 AM
Found In Egroup: Advanced Software
\ view thread
Ok taking it one step at a time. Point #1 trying to display the Web session Counts. I am not very good with coding yet (DotNet) but trying to learn. I am guessing I would need to display the value activeSessions..... If so, How do I get it exposed to the UI. As I see the other two from the screen ...
Posted By Retzlaff Jan 02, 2026 09:04:00 AM
Found In Egroup: Advanced Software
\ view thread
I figured that but wanted to get it posted before I forgot my thought pattern. Thanks for staying engaged @Blake Community. ------------------------------ Scott Retzlaff Automation Engineer | Manufacturing Efficiency Expert | Innovator in Automated Systems ------------------------------
Posted By Retzlaff Dec 31, 2025 01:43:00 PM
Found In Egroup: Advanced Software
\ view thread
Is there a way to display how many web sessions are currently connected and active? Is there a way to pull the PC name via a web session and use that to do certain things. example would be only displaying certain windows based on which PC it is loaded on. i.e. different location on the floor. ...
Posted By Retzlaff Dec 30, 2025 01:20:00 PM
Found In Egroup: Advanced Software
\ view thread
So simple I do not know why I did not see that. Probably because I just did the copy and paste buttons and never thought about it. Works as expected after changes. Thanks! ------------------------------ Scott Retzlaff Automation Engineer | Manufacturing Efficiency Expert | Innovator in Automated Systems ...
Posted By Retzlaff Dec 30, 2025 12:53:00 PM
Found In Egroup: Advanced Software
\ view thread
I created a dialog to use as my clean screen. On that screen I added button that needs to be held for 10 seconds to close which all works as expected. My problem is when it closes there is a blank screen behind it. I would like it to be the Maintenance main page like in the first picture. Steps I would ...
Posted By Retzlaff Dec 18, 2025 11:15:00 AM
Found In Egroup: Advanced Software
\ view thread
Still working on this. The one thing I found that on the Optix Panel that is working correctly the following is the system information. Firmware - 6.0.1.165 OS Version - 8922104A.6.1.0.280 on the optix panel that it is not working is the following: Firmware - 6.0.1.168 OS Version - 8922104A.6.1.1.166 ...
Posted By Retzlaff Dec 16, 2025 10:32:03 AM
Found In Egroup: Advanced Software
\ view thread
I used this to display a warning icon and I like it. It actually moves the text and then when all good the text is center again. Thanks. ------------------------------ Scott Retzlaff Automation Engineer | Manufacturing Efficiency Expert | Innovator in Automated Systems ---------------------- ...
Posted By Retzlaff Dec 15, 2025 08:54:00 AM
Found In Egroup: Advanced Software
\ view thread
I don't think this is possible as I did not see anything, but I may have overlooked something. Is there a way to change the color of one tab on the navigation panel? For instance, I have a permissives screen that if they are trying to start and not all permissives are met it would blink that tab red ...
Posted By Retzlaff Dec 12, 2025 12:48:00 PM
Found In Egroup: Advanced Software
\ view thread
LOL Yes Correct, I copied / created the echart.js file/folder section. And yes I did not download the demo project I did it to my own Optix project. Yes a user defined templeate that I start with for a new project. the .optixz or whatever it is. I am going through different things to check now. ...
Posted By Retzlaff Dec 12, 2025 10:37:00 AM
Found In Egroup: Advanced Software
\ view thread
I guess I am a little confused when you ask the original or the copied one. Originally, I took the sample from GitHub and copied it into my Optix project (creating a "Template". After testing I downloaded it to the Optix panel, and all worked fine. I then took the "Optix Template" and used it for this ...
Posted By Retzlaff Dec 12, 2025 10:04:00 AM
Found In Egroup: Advanced Software
\ view thread
It is weird because it is running perfectly fine on another Optix Panel. Is there something I can compare between the two to try and narrow down my search? ------------------------------ Scott Retzlaff Automation Engineer | Manufacturing Efficiency Expert | Innovator in Automated Systems --------- ...
Posted By Retzlaff Dec 11, 2025 03:25:03 PM
Found In Egroup: Advanced Software
\ view thread
@asemlucben curious on #1 above. Is there a way to connect studio to a panel to monitor for errors without downloading to the panel? ------------------------------ Scott Retzlaff Automation Engineer | Manufacturing Efficiency Expert | Innovator in Automated Systems ------------------------------
Posted By Retzlaff Dec 11, 2025 03:21:20 PM
Found In Library: Advanced Software
Posted By Retzlaff Dec 11, 2025 03:21:00 PM
Found In Egroup: Advanced Software
\ view thread
That makes sense about the "jenkins". I uploaded the logic script by just adding .docx after it for now. The file did not exist under that directory, however I did add it and still no luck. The funny thing is when I run as emulator on my PC it works fine and displays how it should. Just when I download ...
Posted By Retzlaff Dec 11, 2025 08:55:00 AM
Found In Egroup: Advanced Software
\ view thread
I used the example from Github for creating a pareto chart and deployed on one optix panel and all works great. I now have deployed it to another panel, of course with updates pointing to the correct items and it does not work. I am seeing some weird references to a path (jenkins), that I take it is ...
Posted By Retzlaff Dec 11, 2025 08:54:57 AM
Found In Library: Advanced Software
Posted By Retzlaff Dec 05, 2025 11:26:00 AM
Found In Egroup: Advanced Software
\ view thread
I currently have an Optix Panel Standard running connected to an older 1769-L32e (V20) and all looks good, except sometimes it seems like a tag from a toggle button will get stuck high in the PLC. Like it did not see or execute the On Mouse Up Event. I am using a regular button, but it is an exact copy ...
Posted By Retzlaff Dec 02, 2025 08:41:44 AM
Found In Egroup: Advanced Software
\ view thread
Yep, I have used them, but was wondering if there was a center, so I would not have to move the objects back to where I wanted them. They have all the others, just not center. I am sure there is a reason, just seems weird to me not to have it. @asemlucben do you know if this is a future item or the ...