The Cable Track Animator is an unreleased component, but you are free to use it as you like.
This component makes it easy to create an animated Cable Track that animates as associated Visuals experience motion.
The tracking this component provides is SinglePoint per section, which means it is NOT a perfect representation of the way Cable Tracks truly work; however, the effect is convincing enough in most cases.
The attachment is a ZIP file containing two catalogs and an example model.
The two catalogs are the Cable Track Animator component, and catalog of example CAD you can use to follow along with the video below.
Here is a video that walks through how to configure and use the Cable Track Animator.