Automation Control
View Only
Community Home
Discussions
25.9K
Library
1.5K
Members
2.9K
Back to Library
Unable to download to controller. The internal safety partner hardware has failed.
Like
Aug 11, 2021 04:23:04 AM
Dean Willmott
Statistics
0 Favorited
109 Views
2 Files
0 Shares
8 Downloads
Attachment(s)
AB Manual.JPG
99 KB
1 version
Uploaded - Aug 11, 2021
Download
controller fault.png
20 KB
1 version
Uploaded - Aug 11, 2021
Download
Download Document
Please accept the terms of the copyright associated with this attachment before downloading it. Click the link below to read the terms.
Accept
Comments
Mark Givens
Aug 12, 2021 07:36:09 AM
Is it possible you have a "GuardLogix" or safety controller that you are applying in a rack that is not intended for machine safety or safety instrumented system? Is there actually a "safety partner" module installed? Verify catalog/part number of your controller and its associated application/rack installation. If you do have safety controller and it is being applied in rack/application with a safety partner module, then someone else will need to guide, that is not something I have done. Consider engaging tech support by phone also.
Related Entries and Links
No Related Resource entered.
Copyright � 2026 Rockwell Automation. All rights reserved.
Powered by Higher Logic