Hi! I have a physical machine with W7 SP1 64 bits operating system, on this machine ControlFLASCH V15.03 is installed, a virtual machine with the same operating system settings with all software installed. I want to use the serial USB application only on the physical machine, but it is too slow to ...
|