List of Contributions

Justin Lee

Contact Details

Justin Lee


My Content

1 to 8 of 8 total
Posted By Justin Lee Jul 10, 2024 01:45:00 PM
Found In Egroup: Automation Control
\ view thread
The 10 Slot chassis is full. One thought I had: The EN2TR in slot 3 has 4 additional RIO racks and 20ish VFDs. The main redundant chassis have one open slot. Should I, could I, move the slot 3 EN2TR card to the open spot in the main redundant chassis, (yes, I would need one more), then ...
Posted By Justin Lee Jul 10, 2024 10:52:00 AM
Found In Egroup: Automation Control
\ view thread
I didn't design it, I inherited responsibility for this system. Is it possible my unsupported bridged RIO be causing my issues with adding one more analog module? If so, if I increased the RPI on everything in that rack, might my issue go away?
Posted By Justin Lee Jul 09, 2024 11:34:00 AM
Found In Egroup: Automation Control
\ view thread
Slot 0, Eth_Node56 has an RPI of 10 ms. Slot 3, vlan_21Net RPI is grayed out. The EN2TR in slot 3 connects 4 additional EN2TRs (remote I/O chassis) and 20 PF525s. Is using an RIO chassis to connect to more RIO chassis acceptable?
Posted By Justin Lee Jul 09, 2024 11:33:46 AM
Found In Library: Automation Control
Posted By Justin Lee Jul 09, 2024 08:32:00 AM
Found In Egroup: Automation Control
\ view thread
Nothing is set to unicast, as per redundant system requirements. CPU seems fine. Multicast Producers is maxxed out. Is that my underlying issue? Is there a way to reduce that, or increase the max supported?
Posted By Justin Lee Jul 09, 2024 08:31:33 AM
Found In Library: Automation Control
Posted By Justin Lee Jul 08, 2024 02:31:23 PM
Found In Library: Automation Control
Posted By Justin Lee Jul 08, 2024 02:31:00 PM
Found In Egroup: Automation Control
\ view thread
We've got a large system, 2 - L71's, ver24, running redundant. It has a 10 slot chassis for remote I/O. Slot 7 was empty, so we added a IF16. When active, it faults out, "(16#0002) Resources Unavailable". I read something that pointed me towards the 1756-EN2TR card that connects this RIO to the PLC ...