List of Contributions

ÖZSU

Contact Details

ÖZSU


My Content

1 to 20 of 31 total
Posted By ÖZSU Jun 03, 2026 07:30:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hello everyone. I am currently working on an application using SQL Server Management Studio (SSMS) and FactoryTalk Optix. I am attaching the screenshots of my current setup. On Optix, I successfully created an ODBC Database and connected it to my SQL Server. When I add or remove a column within this ...
Posted By ÖZSU May 13, 2026 12:48:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
I solved the problem. While on the P1800 screen, I pressed the # key and typed 40050, and it worked. -------------------------------------------
Posted By ÖZSU May 12, 2026 08:33:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Hello everyone, I am currently working with a PowerFlex 755TS drive. I wanted to set up a simple application using a potentiometer and a switch. I can successfully issue start/stop commands, but I cannot change the speed using the potentiometer. What I need to do is set the value of Port 10 : Parameter ...
Posted By ÖZSU May 11, 2026 08:39:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
The issue I described above is a problem the customer is experiencing. I successfully established communication in the office using a Micro850 PLC via the ETH2 port. We know we can communicate through the ETH2 port, so what could be causing the problem on the customer's end? ----------------------- ...
Posted By ÖZSU May 11, 2026 08:37:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
I am connecting to the ETH1 port via Siemens TIA Portal over ProfiNet, and it is working. There was no problem communicating with the Siemens PLC. I am setting up communication with the CompactLogix PLC via the ETH2 port. I can import the tags, but when I assign them to buttons and LEDs, I get a communication ...
Posted By ÖZSU May 11, 2026 07:31:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hello, We are experiencing a network communication issue with our FactoryTalk Optix panel. When I connect Port 2 (on the 192.168.1.XX subnet), I can successfully ping the panel and read PLC tags. However, despite this, the panel does not show up in Linx (RSLinx/FactoryTalk Linx). On the other ...
Posted By ÖZSU Apr 17, 2026 08:17:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi everyone. I'm currently implementing a DataGrid in Optix with 5 pre-defined objects bound to it. My goal is to dynamically add and edit rows and columns programmatically while the application is running. Is it possible to perform these dynamic modifications at runtime? ---------------------- ...
Posted By ÖZSU Apr 15, 2026 02:31:04 AM
Found In Library: FactoryTalk Optix
Posted By ÖZSU Apr 15, 2026 02:31:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
I have solved the previous issue. However, I have another question. I want to write the date and time to PLC tags and have them visible in the PLC tags during Runtime. I added ClockLogic time to the PLC tags using a dynamic link. I can see the time and date in the tags during Runtime, but I am getting ...
Posted By ÖZSU Apr 14, 2026 05:07:25 AM
Found In Library: FactoryTalk Optix
Posted By ÖZSU Apr 14, 2026 05:07:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
I solved the previous issue, but now I'm facing a new one. I have two local languages in my project, Turkish and English, and I switch between them. While the alarm message is displayed correctly in the alarm section, it does not appear in the alarm history (as shown in the images). When I change (Item)/Message ...
Posted By ÖZSU Apr 14, 2026 12:54:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
In the screenshot, it appears as 'AlarmsEventLogger1', but it is actually 'AlarmsEventLogger' in my project. I made a typo in the description. -------------------------------------------
Posted By ÖZSU Apr 14, 2026 12:26:08 AM
Found In Library: FactoryTalk Optix
Posted By ÖZSU Apr 14, 2026 12:26:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
In my Optix project, the real-time Alarms section functions correctly; however, I am encountering an error in the Alarm History section. Setup Details: Database: Created an embedded database named DB_Alarms. Logger: Assigned this database to the AlarmEventsLogger object. Query Attempted: ...
Posted By ÖZSU Apr 08, 2026 04:34:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
I solved the problem and it's working exactly as I want it to now. -------------------------------------------
Posted By ÖZSU Apr 02, 2026 01:02:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hello. I followed your instructions, but it's still not working the way I want. The recipe list is numbered 1, 2, 3, etc., but the recipes names aren't displayed. I can upload the recipes to the PLC and retrieve them from the PLC. The only problem is that the recipes names aren't listed.