List of Contributions

⚙ Andre Yost

Contact Details

⚙ Andre Yost


My Content

1 to 20 of 33 total
Posted By ⚙ Andre Yost Mar 05, 2026 08:20:00 AM
Found In Egroup: Emulate3D Software
\ view thread
Hi Slejska, Given what you've shared, all info points to something specific to your model causing problems. (I just successfully saved a model with people in it using the versions you'd used.) At this stage, I'm assuming the following: You have some custom script that somehow references ...
Posted By ⚙ Andre Yost Mar 03, 2026 01:54:00 PM
Found In Egroup: Emulate3D Software
\ view thread
Hi Slejska, At a first pass given your provided info, your troubles seems like one due to potential issues with versioning, caching, or a bad script. Try working through the below Qs and see if that yields any results. Which versions of Emulate3D and the People's catalog are you using? ...
Posted By ⚙ Andre Yost Feb 16, 2026 10:42:00 AM
Found In Egroup: Emulate3D Software
\ view thread
Hi all! Two points to add here. Consider converting your models/catalogs to their XML variants (File -> Save As)! This allows you to access & modify scripts directly without needing to navigate to any temporary directory. This is also the preferred filetype for any Git based versioning since ...
Posted By ⚙ Andre Yost Jan 15, 2026 02:14:00 PM
Found In Egroup: Emulate3D Software
\ view thread
Hi Andy, For the PLC internal timing, I believe you are interpreting this correctly and I stand corrected; I'll be running this past our team. Thank you for diagnosing the situation so thoroughly! Edit: I'll add that I was rechecking our page for Connecting to FT Logix Echo, and I noted that ...
Posted By ⚙ Andre Yost Jan 15, 2026 12:36:10 PM
Found In Library: Emulate3D Software
Posted By ⚙ Andre Yost Jan 15, 2026 12:36:00 PM
Found In Egroup: Emulate3D Software
\ view thread
Hi Nemo! Succinctly, you're absolutely correct; there is no built-in feature for Baggage Handling conveyors (or any other Emulate3D out of the box conveyors in other catalogs) to track the loads on them, because conveyors have a Body Type = Deflector, while PEs have a Body Type = Sensor. ...
Posted By ⚙ Andre Yost Jan 06, 2026 08:49:00 AM
Found In Egroup: Emulate3D Software
\ view thread
Hi Andy, Happy New Year! Glad I could be of help with the first question, & now I fully understand the nuances of your second. Today, Emulate3D only accesses existing controller/program scoped tags. In other words, if some PLC property/variable is internal (meaning that no tag holds that p ...
Posted By ⚙ Andre Yost Jan 02, 2026 10:43:00 AM
Found In Egroup: Emulate3D Software
\ view thread
Hi Ruiz, To start, verify that you are using the latest version of Emulate3D. If not, upgrade & see if the exception persists. If that does not work, please provide some additional info: Studio 5000 version Logix Echo version Controller catalog number Controller version ...
Posted By ⚙ Andre Yost Jan 02, 2026 10:29:00 AM
Found In Egroup: Emulate3D Software
\ view thread
Hi Andy, I recommend opening a ticket with support to help diagnose the issue. Based on any findings therein, we will update this thread. Thanks! ------------------------------ ⚙ Andre Yost Emulate3D ------------------------------
Posted By ⚙ Andre Yost Jan 02, 2026 09:45:00 AM
Found In Egroup: Emulate3D Software
\ view thread
Hi Andy, hope you're well. Q1: Succinctly yes, the device based alarm's internal timers can be configured to be lockstep with any model speed. Once you set up a co-simulation connection between your model & PLC, any PLC execution will be lockstep with any Emulate3D model run speed / stop interactions. ...
Posted By ⚙ Andre Yost Dec 04, 2025 10:31:00 AM
Found In Egroup: Emulate3D Software
\ view thread
Hi Loganathan, Without having all the details about your model, I'd try the approach of reparenting the tire to the vehicle so that when the vehicle position is manipulated, the tire locations follow. This reparenting action can be achieved using either C# or quick logic, which is executed after some ...
Posted By ⚙ Andre Yost Nov 06, 2025 08:52:00 AM
Found In Egroup: Emulate3D Software
\ view thread
Hi Joey, I'm glad that worked! As for your question, you will need a fully licensed Emulate3D software installation to properly run plugin commands. This is because those CLI calls rely on the same Emulate3D services that run in the background on your machine, and those services are packaged with ...
Posted By ⚙ Andre Yost Nov 03, 2025 09:19:00 AM
Found In Egroup: Emulate3D Software
\ view thread
Hi Joey! Specify the license group as another argument, like exampled below: & $EMULATE3D_PATH plugin Emulate3D.PackageTools --serialno $SERIALNO --packagefeed "$PACKAGE_FEED" --pluginargs -- "script --scriptname $SCRIPT_NAME --containerpath $PACKAGE_PATH --packagepath $SCRIPT_PROJECT --commitfeed ...
Posted By ⚙ Andre Yost Oct 31, 2025 07:04:00 AM
Found In Egroup: Emulate3D Software
\ view thread
Hello, hello! Expanding on the other great responses here, I'll reiterate that to force the value of the server item (what you have circled above), you'll need to access the relevant BindableItem. Example code summary: The custom simple property has an associated event firing whenever the property ...
Posted By ⚙ Andre Yost Oct 28, 2025 08:06:00 AM
Found In Egroup: Emulate3D Software
\ view thread
Hi Frank, I second all the thorough responses above, only adding a brief shoutout to some of the other public resources that are available for training/troubleshooting. Cheers! GitHub repository (ra-emulate3d-core-samples) contains great examples of scripted, custom behaviors. YouTube ...
Posted By ⚙ Andre Yost Oct 23, 2025 03:37:00 PM
Found In Egroup: Emulate3D Software
\ view thread
Hi Joey, You're diving into a topic that our own team is currently and actively looking into! I'll start by answering your question directly, then include some additional CI/CD resources below that you may find interesting. Is it possible to automate this action so that when I merge the ...
Posted By ⚙ Andre Yost Oct 10, 2025 03:26:00 PM
Found In Egroup: Emulate3D Software
\ view thread
Hello Quyen! The below solution showcases the use of c# scripting to control the behavior of visuals from the people catalog. A model + video are attached. Notably, it is important to emphasize that the primary driver of custom behavior for the People catalog is implemented through QuickLogic. ...