List of Contributions

Caskey

Contact Details

Caskey


My Content

1 to 3 of 3 total
Posted By Caskey Mar 25, 2024 03:53:00 PM
Found In Egroup: Automation Control
\ view thread
Hi, I'm trying to connect a Huracan digital gauge surface module to an existing MVI156E module via Modbus. The Huracan module is showing valid readings. There are existing modbus connections utilising the PLC module and I've been able to figure out most of the settings however the connection still ...
Posted By Caskey Jan 07, 2024 04:00:00 PM
Found In Egroup: Automation Control
\ view thread
When adding a routine in RS Logix I haven't been able to change the sheet size to a suitable size. The work around I use is to save a routine which is of a suitable size then import that routine. Hopefully a simple answer to this. Cheers EDIT: moved to Automation Control community -FL - ...
Posted By Caskey Dec 04, 2023 01:25:00 PM
Found In Egroup: Advanced Software
\ view thread
I have a couple of old PC's here being used as FT operator consoles which I want to replace. These things don't even have wifi capability so anything reasonable in the second hand line will probably do the trick and be a big improvement. I was wondering what the minimum spec is for this type of usage. ...