List of Contributions

TysonQCA

Contact Details

TysonQCA


My Content

1 to 6 of 6 total
Posted By TysonQCA Oct 14, 2025 07:34:00 PM
Found In Egroup: Automation Control
\ view thread
Hi Defreitas, Maybe you will need to change the filename (Path) in the logix designer project that you download to the PV as well. -------------------------------------------
Posted By TysonQCA Feb 13, 2025 04:23:00 PM
Found In Egroup: Automation Control
\ view thread
Doubt it, considering the RM2 communicates through the bus. But you can try. A power cycle after assigning IP may do the trick. Let me know.
Posted By TysonQCA Feb 13, 2025 03:39:00 PM
Found In Egroup: Automation Control
\ view thread
Power Down One Chassis: Start by powering down one of the redundant chassis. This ensures that only one chassis is active at a time, preventing IP conflicts during the configuration process. Remove the Redundancy Module: Remove the 1756-RM2 module from the active chassis. This step is crucial ...
Posted By TysonQCA Feb 13, 2025 03:37:00 PM
Found In Egroup: Automation Control
\ view thread
you need to set one to .10 and the partner incremented by 1 ie .11 They cant be the same but the RM2 will handle the changeover.
Posted By TysonQCA Oct 02, 2024 11:38:00 PM
Found In Egroup: Automation Control
\ view thread
Hi John, In logix designer is the module configured to be single ended or differential current? You are likely correct that the problem is ground loops, depending if you can afford to lose the capacity, set the 1756-IF16 as differential current input, meaning each channel has an isolated RTN. ...