Posted By
Tim K
Jul 27, 2026 07:27:14 AM
Found In
Egroup:
FactoryTalk Optix
\
view thread
Hi, I'm wondering the best way to handle large Logix array UDTs. I have 2 PLC tags which, when imported as the full UDTs, end up producing ~6 million nodes. The majority of these nodes are from the generated array index tag structures. Two questions: Previous Optix versions would create the ...
|