List of Contributions

KAJ

Contact Details

KAJ


My Content

1 to 20 of 50+ total
Posted By KAJ Nov 01, 2024 09:12:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Thanks god Finally ! i will test the script and see if it works as i thought.
Posted By KAJ Oct 30, 2024 03:45:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hello, I'm still struggling to save a recipe file via FTP. Has anyone successfully transferred a CSV file without using FTP? I'm looking for a simple and stable way to do this over a LAN.
Posted By KAJ Sep 25, 2024 03:24:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Thanks for update!,
Posted By KAJ Aug 28, 2024 02:32:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
In my experience, I don't recommend using FTP as it causes communication loss every time. I spoke with Rockwell support, but they didn't investigate the issue because I don't have a TechConnect contract.
Posted By KAJ Aug 21, 2024 08:30:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Thanks!, I solved the issue by copying the complex dynamic link tand link it to the variable in the model folder. I wasn't sure if it would work because I couldn't access the UI from the model variable, but when I search for the variable from my container, it finds the model folder and accesses the ...
Posted By KAJ Aug 21, 2024 08:00:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
I have text box called calculate and it contain complex link that have expressesion evaluator , what i want to achive is to send that value to a variable in the model folder, Total value 100 is the variable value in the text box beneath the calculate.
Posted By KAJ Aug 21, 2024 05:19:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hello, What I want to achieve is to send the value from the UI box to Model/Var1. I tried this method, but it only works if you manually change the value in the UI box (Calculate). I'm not sure if this is the intended behavior or if it's a bug.
Posted By KAJ Jul 26, 2024 03:03:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
1. I hope that soon Optix can open tabs in new windows because having everything in one place and using split view is a useless function if it doesn't work independently. 2. When selecting multiple UI elements to change properties of their visibility, you can only change them to True or False and ...
Posted By KAJ Jul 05, 2024 08:21:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
When I try to drag and drop any object from the library into my project, the program closes. I haven't experienced this with the older version. I am using V 1.4.0.938.
Posted By KAJ May 31, 2024 08:03:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
@asemlucben @Philip Hamilton
Posted By KAJ May 29, 2024 09:03:25 AM
Found In Library: FactoryTalk Optix
Posted By KAJ May 29, 2024 09:03:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Yeah, its nice to change the backround picture from time to time :)
Posted By KAJ May 29, 2024 02:05:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Posted By KAJ May 23, 2024 01:37:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hello, I've created a periodic action for when the FTP client is disconnected from the server. It works fine in the beginning, but after some hours, I lose communication with the server. The script should attempt to reconnect to the server every 3 seconds if no connection is established. Filezilla ...
Posted By KAJ May 17, 2024 07:29:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
I wonder if this is the way this split window should work. It would be more useful if you could keep the second window separate from the first one when selecting objects. It's quite slow to add variables in this way, and you can't even search for reference addresses like in the old FTOPTIX version. Any ...
Posted By KAJ May 15, 2024 07:40:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
I solved the issue by the code of Shane and i attached every .net script to every textbox
Posted By KAJ May 15, 2024 07:32:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
In my case, I want to change the value that is created by the recipe schema in Optix from a tag in the PLC.
Posted By KAJ May 15, 2024 07:27:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
I can't delete these blank lines in the recipe name. It happened after I made some changes in the CSV file and imported it back. It's affected all the other projects I have in Optix. Why?
Posted By KAJ May 14, 2024 06:19:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Yes, in my case the value is dynamic so the best option will be with NetLogic
Posted By KAJ May 13, 2024 08:16:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Thanks, Shane i solved the 1 point, and for the 3 one i created a periodic action to reconnect to the server when the ftpclientisrunning is 0