Hello All, I have a recently installed refurbished PF700 that has an issue with starting up in the mornings. When the motor is started it could run for 30 seconds to 5 minutes and the Drive Status Ready bit will drop out for a split second, but this causes the motor to stop. No faults are present ...
|