List of Contributions

Morella

Contact Details

Morella


My Content

1 to 5 of 5 total
Posted By Morella Jun 30, 2025 08:24:00 AM
Found In Egroup: Automation Control
\ view thread
I want to set the Hard Fault setting to "Restart controller automatically" in case a hard fault occurs. is there a way to trap the fault code so that when the PLC re-starts I can report the fault on the HMI? I am using CCW 22.00.00
Posted By Morella Oct 21, 2024 12:37:00 PM
Found In Egroup: Automation Control
\ view thread
It is a 2080-TC2 plug-in module mounted next to a 2080-OW4I module. I will try adding the PLUGIN_RESET function if the __SYSVA_MAJ_ERR_HALT tag is set. Is this something I can do from within the normal program sequence, or does it require some sort of exception handling code?
Posted By Morella Oct 21, 2024 09:38:00 AM
Found In Egroup: Automation Control
\ view thread
I am trying to troubleshoot an intermittent situation where an analog input module is creating a major fault. if I were able to automatically reset the PLC, it would give me more options while troubleshooting.
Posted By Morella Oct 21, 2024 07:40:00 AM
Found In Egroup: Automation Control
\ view thread
Is there a way to automatically reset the Micro820 PLC if there is a fault? I am using CCW version 22 EDIT: moved to Automation Control community -FL
Posted By Morella Oct 17, 2022 02:48:00 PM
Found In Egroup: Automation Control
\ view thread
EDIT: moved to Automation Control community -FL I want to be able to access the Ethernet port's IP configuration from an HMI that is connected to the Micro820's serial Modbus RTU port. Otherwise, i have no way of knowing what the IP settings are. Is there a way to read the Micro820's IP configuration ...