List of Contributions

Torrild

Contact Details

Torrild


My Content

1 to 5 of 5 total
Posted By Torrild Aug 04, 2026 07:20:29 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Neither 10000 or 3567587328 worked :O ------------------------------ ____________________________ Best Regards, Peter Kjær Torrild ------------------------------
Posted By Torrild Aug 04, 2026 06:38:30 AM
Found In Egroup: FactoryTalk Optix
\ view thread
I have currently set it to HTTP and increased the number of max connections to from two to five. Still the connection refused error persist. I am running this on a OptixEdge 2800E which i should have included in my original post. ------------------------------ ____________________________ Best Regards, ...
Posted By Torrild Aug 04, 2026 05:15:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Hi everyone, I have a web presentation engine where, Link 1 is set to DHCP and get a correct address (I can open the configuration manager) and Link 2 is set to a static IP-Address. Here I can correctly access the session using the static IP on the LAN (LINK2), however, I cannot access the session ...
Posted By Torrild Aug 04, 2026 04:02:20 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Just in case anyone else wants to do something similar, I did eventually get a runtime implementation working. As @asemlucben correctly explained, it was not possible to add tags dynamically at runtime through the integrated OPC UA client. The integrated client expects its tag structure to be defined ...
Posted By Torrild Jun 17, 2026 01:18:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
I am working in FactoryTalk Optix and need to dynamically add/import an OPC UA tag to an arbitrary OPC UA client during runtime, based on a path entered by the operator/HMI. The goal is not to preconfigure all tags at design time. The requirement is that the runtime application can receive or type ...