Posted By
HubP_WHo
Oct 09, 2025 03:04:54 AM
Found In
Egroup:
Emulate3D Software
\
view thread
Hi JadhaV, This kind of mechanism is possible when you add the right Joins and set the right Bases. In fact, the object A seems to need 2 Revolute Joints: one should have the Object B as Base, and the second one with the Object B as Base. Note that, a base of a Joint can't be the visual on which ...
|