List of Contributions

Gazzag

Contact Details

Gazzag


My Content

1 to 8 of 8 total
Posted By Gazzag Dec 18, 2022 05:46:00 AM
Found In Egroup: Advanced Software
\ view thread
Hi @Flockhart You can do this with 'Runtime Security' and uses the security codes assigned to each user, I assume you have pages that can only be accessed when certain user groups log in, these are assigned the security codes A - P depending on access on the display icon use for example - CurrentUserHasCode( ...
Posted By Gazzag Dec 18, 2022 01:48:00 AM
Found In Egroup: Automation Control
\ view thread
Hi, how does the HMI set the SSV, is this a user enterable value? do you have a few pictures showing the code in the PLC with respect to the tags/logic that you can share? G ------------------------------ Goodall ------------------------------
Posted By Gazzag Dec 06, 2022 08:34:00 AM
Found In Egroup: Advanced Software
\ view thread
Hi @fuzzy logic Result! yes that is what was stopping the connection, just changed to the computers IP and all working thanks for you help​ ------------------------------ Goodall ------------------------------
Posted By Gazzag Dec 05, 2022 03:44:00 AM
Found In Egroup: Advanced Software
\ view thread
Hi Fuzzy Logic, I have attached a few files to show the current setup, the processor path was .6 (not 2.15 my mistake) No managed switches on the system, connection directly to a unmanaged switch in the local panel from the CPX to PC and local panelview plus 7. Ping is successful from the PC and using ...
Posted By Gazzag Dec 05, 2022 03:43:56 AM
Found In Library: Advanced Software
Posted By Gazzag Dec 01, 2022 03:29:00 PM
Found In Egroup: Advanced Software
\ view thread
Thanks for the reply. I tried using the 172.16.11 15 as the browse address but the connection indicator stays black, is there anything else I can check that would be causing the source connection issue. Works with another driver so no hardware issues, but cannot connect using CIP Ethernet/ip. CIP connections ...
Posted By Gazzag Dec 01, 2022 03:28:46 PM
Found In Library: Advanced Software
Posted By Gazzag Dec 01, 2022 01:24:00 PM
Found In Egroup: Advanced Software
\ view thread
Hi All, I am just trying to configure a data source in the gateway server to connect my local laptop to a compactlogix 5069 L340er controller, using smart objects model, v32 .acd project file Set the CIP driver path to the controller so my browse path is 172.16.11.15 (processor) but I realise i need ...