List of Contributions

Rosby

Contact Details

Rosby


My Content

1 to 14 of 14 total
Posted By Rosby May 08, 2025 06:16:00 AM
Found In Egroup: Advanced Software
\ view thread
Thanks you very much, it greatly help
Posted By Rosby May 07, 2025 08:42:00 AM
Found In Egroup: Advanced Software
\ view thread
How do you make a file to have the data?
Posted By Rosby May 06, 2025 10:38:00 AM
Found In Egroup: Advanced Software
\ view thread
Hi, As anyone try to export all the tags used by the HMI? Because I try via Tools > Tag Import and Export Wizard to have empty list and I am using a lot of Global Object. It is a project made by another company and they don't know anything and I am trying to log the value in a Database for the trends ...
Posted By Rosby Nov 27, 2024 01:35:00 PM
Found In Egroup: Advanced Software
\ view thread
Hi, I am trying to make open a display when a tag is equal 1, but in the client I get the error : 'The command 'Display' is ignored when issued from the development environment or an HMI Server.' and the display don't open and I have try with Events from the Logic and Control and that call the macro ...
Posted By Rosby Nov 23, 2023 07:29:00 AM
Found In Egroup: Advanced Software
\ view thread
Hi, In FactoryTalk View SE Network Distributed I can connect and see the tags from my automate model 1785-L40B in PLC5, but I can't see tags bits like N26:7/14 I will only see the N26:7.And even try to add it manually but no success. Do somebody got this problem too or know the solution? ---- ...
Posted By Rosby Sep 28, 2023 05:01:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
Thanks you ------------------------------ Rosby ------------------------------
Posted By Rosby Sep 27, 2023 12:27:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
I have a project in FactoryTalk Network and I can't connect to my Kepware via OPC UA I always get the error that it can't find the endpoint with "Failure retrieving endpoints from url, error: "BasSequenceNumberInvalid" " and "Failed to get desired endpoint for "url enpoint": "BadNoMatch" ". But ...
Posted By Rosby Sep 20, 2023 09:41:00 AM
Found In Egroup: Advanced Software
\ view thread
I want to connect my project FactoryTalk View Talk Machine Edition to a second OPC DA server from another pc with Kepware even if my DCOM is working with OPC Client FactoryTalk Studio always get the error 80000003 why? I already try with setting the DCOM with MSDCOMHardeningManagement and SetRnaDCOMLevel ...
Posted By Rosby Sep 05, 2023 05:03:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
I am using the IP address and both of are not in a DNS. I forget to mention one is a windows server and the other a windows 10 (FactoryTalk installed on this one) could it be a problem? (They are both offline, not connected to the ethernet) The only error I got is this one: Failed to connect to browse ...
Posted By Rosby Sep 01, 2023 01:42:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
Unfortunately my windows is too much up to date, but I still use the one to set DCOM Auth level to Packet Integrity and I still have the same error. My goal is to have a second OPC server in my project Machine Edition on a remote Kepware server, I setup my DCOM like the Kepware procedure and I know ...
Posted By Rosby Sep 01, 2023 12:43:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
I have the patch from july 2023 for FTView v12 ------------------------------ Rosby ------------------------------
Posted By Rosby Sep 01, 2023 12:28:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
I see the Keys in the registry at five, but still not working, both my pc are to 2023 version ------------------------------ Rosby ------------------------------
Posted By Rosby Sep 01, 2023 08:14:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
First I don't find HKEY_LOCAL_MACHINE\SOFTWARE\Rockwell Software\FactoryTalk\Platform\DCOMAuthLevel or HKEY_LOCAL_MACHINE\SOFTWARE\WOW6432Node\Rockwell Software\RSLinx\DCOMAuthLeve I am using the FactoryTalk View V12 Machine Edition and I am supposed to put the Authentication ...
Posted By Rosby Aug 31, 2023 01:03:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
I got two computer, both of them have a OPC server Kepware, one have an alarm software and the other one have FactoryTalk View Studio Machine Edition I both setup the DCOM and both with OPC client can access to each other tags in the OPC server Kepware, but I can connect to each other OPC server from ...