List of Contributions

Josh Broselle

Contact Details

Josh Broselle


My Content

1 to 16 of 16 total
Posted By Josh Broselle Jul 19, 2022 09:23:00 AM
Found In Egroup: Legacy
\ view thread
It's been put on the back burner for now, lot's of other stuff going on. I added in the 15 second TON back to the program so we could run both pumps. All alarms work and functions as it should. When I find a solution I will post up on what solved it. Sorry for keeping people in the dark for a wh ...
Posted By Josh Broselle Jul 05, 2022 12:03:00 PM
Found In Egroup: Legacy
\ view thread
Well changing out the timer and just running the pump when the float makes contact did not change anything. Back to the drawing board.
Posted By Josh Broselle Jul 05, 2022 10:57:00 AM
Found In Egroup: Legacy
\ view thread
This is how they do their programs here. "REMOTE" being through SCADA and "HAND" being run
Posted By Josh Broselle Jul 01, 2022 05:06:00 PM
Found In Egroup: Legacy
\ view thread
Will do. Hope to get to it next week
Posted By Josh Broselle Jul 01, 2022 01:52:00 PM
Found In Egroup: Legacy
\ view thread
sorry for the delay..... yes HOA for both pumps. (REMOTE = Auto , and HAND = Pump run) I'm going to try and take the timer out and see what happens
Posted By Josh Broselle Jun 30, 2022 05:20:00 PM
Found In Egroup: Legacy
\ view thread
I can't see the message on the forum here, but thank you for looking.
Posted By Josh Broselle Jun 30, 2022 02:02:00 PM
Found In Egroup: Legacy
\ view thread
@Splash here it is.... Thank you
Posted By Josh Broselle Jun 30, 2022 02:01:58 PM
Found In Library: Legacy
Posted By Josh Broselle Jun 30, 2022 01:05:00 PM
Found In Egroup: Legacy
\ view thread
I'm trying to get the RSS file on the computer I'm working on currently. Thank you
Posted By Josh Broselle Jun 30, 2022 09:40:00 AM
Found In Egroup: Legacy
\ view thread
(If I understand you correctly, you are seeing both I:0/5 and I:0/8 (Pump 1 Run & Pump 2 Run) come on, but you are expecting only Pump 2 to run.) No sorry I will try and explain better..... So when both pumps are in AUTO and the request is set to run the pumps, then the RUN command or "HAND" also ...
Posted By Josh Broselle Jun 30, 2022 09:40:00 AM
Found In Egroup: Legacy
\ view thread
EDIT: manually quoted the text so that it's clearer -FL If you could upload the program - I'd be happy to look. You have to have something else writing to it somewhere. Personally I enjoy these quests. How do we do this?
Posted By Josh Broselle Jun 29, 2022 04:52:00 PM
Found In Egroup: Legacy
\ view thread
Yes the inputs I:0/5 and I:0/8 both engage and run like it's in manual operation or run mode
Posted By Josh Broselle Jun 29, 2022 03:22:00 PM
Found In Egroup: Legacy
\ view thread
it's both pumps that do the same thing, not just pump 2
Posted By Josh Broselle Jun 29, 2022 03:19:00 PM
Found In Egroup: Legacy
\ view thread
it's a b9:0/8
Posted By Josh Broselle Jun 29, 2022 02:58:00 PM
Found In Egroup: Legacy
\ view thread
Yes I was getting to that, sorry all. This is where I inserted the 15 second timer Nothing here changed, but now when in "AUTO" or remote, the run input also makes.
Posted By Josh Broselle Jun 29, 2022 02:19:00 PM
Found In Egroup: Legacy
\ view thread
Hello all, New to the PLC world and am a little stuck on something that I'm thinking is super simple, but I can't find the solution. I recently added a TON timer to a second motor to delay the start by 15 seconds. After making the change and reloading the program, it now activates a second "input". ...