List of Contributions

Ian Shaw

Riverside Automation

Contact Details

Riverside Automation
61 Wostenholm Road
Nether Edge
Sheffield
United Kingdom
Google Map Icon

Ian Shaw


My Content

1 to 20 of 50+ total
Posted By Ian Shaw Jun 26, 2026 04:01:00 AM
Found In Egroup: Automation Control
\ view thread
Hi Joao, The timestamp is stored as a LINT (64 bits) . You should be able to just subtract two values. If your controller is old then the SUB instruction may not support LINT. There is an AOI called L_SUB in the Process Library, I believe. https://compatibility.rockwellautomation.com/Pages/D ...
Posted By Ian Shaw Mar 03, 2026 04:33:00 AM
Found In Egroup: Automation Control
\ view thread
Have you considered using arrays of tag-based alarms or ALMD instructions for your various categories? You could then use indexing instructions, such as in FOR loop to for example: Count the the .InAlarm flags. Find the highest .Severity that is .InAlarm. Compare a Warning array with ...
Posted By Ian Shaw Feb 23, 2026 03:53:00 AM
Found In Egroup: Automation Control
\ view thread
To echo what @kurt klingbeil wrote, Modbus Registers start at 1 but Modbus Addresses start at 0. This can often lead to a discrepancy when manufacturers document their data table. They often don't say which they are using, or get their own terminology wrong. This can lead the request being off ...
Posted By Ian Shaw Feb 10, 2026 07:37:00 AM
Found In Egroup: Automation Control
\ view thread
To add to @Philip Hamilton wrote, you should look at your program to see how the PID instruction is being triggered. Is it in a timed or continuous task? Is it triggered by a timer? Is the PID configured with an update rate that is compatible with the rate it is actually being updated? A couple ...
Posted By Ian Shaw Dec 17, 2025 04:07:00 AM
Found In Egroup: Automation Control
\ view thread
Move the timestamp you want to an ALMD or ALMA .ProgTime and set the .UseProgTime input. Digital Alarm (ALMD) Instruction Help UseProgTime BOOL Specifies whether to use the controller's clock or the ProgTime value to timestamp alarm state change events. ...
Posted By Ian Shaw Dec 04, 2025 05:19:00 AM
Found In Egroup: Automation Control
\ view thread
TL;DR Set your SCL_01 to output 4000-2000. Set your OF8C to Engineering Units. As a general principle, break the problem in two to find out whether you have a hardware or software issue. Then break that part into smaller bits until you've eliminated all the parts that function correctly. ...
Posted By Ian Shaw Nov 12, 2025 08:43:00 AM
Found In Egroup: General Discussions
\ view thread
Hi all, I'm a Londoner by birth but have spent my career in Sheffield. ------------------------------ Ian Shaw Riverside Automation, Sheffield, UK If I've helped you, please Like or mark as Best Answer ≈≈≈≈≈≈≈≈≈≈≈≈≈≈≈≈≈≈≈≈≈≈≈≈≈≈≈≈≈≈≈≈≈≈≈≈≈≈≈≈≈≈ ------------------------------
Posted By Ian Shaw Oct 20, 2025 05:55:00 AM
Found In Egroup: Automation Control
\ view thread
There are two really useful tips in @Philip Hamilton's post #8 that I didn't know. That there IS a way to update UDT details during run mode, even if there are limitations. That you can temporarily change the tag external access = NONE to get around HMI or SCADA blocking your attempt to change ...
Posted By Ian Shaw Oct 17, 2025 11:58:00 AM
Found In Egroup: Automation Control
\ view thread
Hi Michael, @Philip Hamilton is from Rockwell whereas I am not, so you should probably consider his answer as official. Having said that, the main reasons my file looks more complex is: I've populated 32 bits compared to his 9. I've added Descriptions to some of my bits, each ...
Posted By Ian Shaw Oct 17, 2025 11:06:00 AM
Found In Egroup: Automation Control
\ view thread
@Philip Hamilton beat me to it! Still, it's been fun to play around with it. I've attached a UDT file you can play with and import. Setting a BOOL sets the equivalent bit in the Overlay DINT. And here's an example of ladder addressing the bits directly, and using an index to select a bit in ...
Posted By Ian Shaw Oct 06, 2025 06:43:00 AM
Found In Egroup: Legacy
\ view thread
Thanks for the confirmation of Philips answer, Jason. Sometimes we might be able to use a client's license, but I suspect that they would usually be unhappy to rehost it to a PC in our office for the duration of a project while they have production PLCs they need to support. It's an avenue we will ...
Posted By Ian Shaw Sep 29, 2025 05:35:00 AM
Found In Egroup: Legacy
\ view thread
We've received an email from our distributor of 26 September about RSLogix 5 End of Life on 31st December 2025, which states that "RSLogix™ 5 software will not be included in your next Enterprise Toolkit renewal". Please could somebody clarify whether we will still be able to use our Toolkit Licence ...
Posted By Ian Shaw Sep 18, 2025 03:28:00 AM
Found In Egroup: Automation Control
\ view thread
This looks like only a display issue. 9.74655151e-04 ≡ 0.000974655151. Your Command and Actual Position are close enough that they are equal to 5 decimal places. Even though they are showing the same on the screen, they probably differ slightly at higher precision. The processor itself works with ...
Posted By Ian Shaw Sep 01, 2025 04:28:00 AM
Found In Egroup: Automation Control
\ view thread
Hi Mooki, You haven't given enough detail for anyone to be able to help you. For instance, you haven't said what version of FactoryTalk you are using, so nobody can advise on compatibility. Try putting the products you are thinking of using into the Product Compatibility and Download Centre ...
Posted By Ian Shaw Aug 13, 2025 05:06:00 AM
Found In Egroup: Automation Control
\ view thread
This is a great question. I've had to field similar questions from operators. Telling them, "Oh, that's just how Rockwell decided to label all digital alarms" isn't a wonderful answer. Many people would like to change that description. But I think that TRIP is a fixed category along with HIGH, LOW, ...
Posted By Ian Shaw Aug 08, 2025 06:21:00 AM
Found In Egroup: Automation Control
\ view thread
I've not used Ignition but I'd be surprised if a modern HMI can't read elements of a Rockwell tag. Try setting a TON.PRE or reading an .ACC. The principle should be the same. It may only work if the tag is in the Controller scope. Or, you may have to add extra syntax like Program:MyProgram!MyPide.CV. ...
Posted By Ian Shaw Jul 25, 2025 04:50:00 AM
Found In Egroup: Automation Control
\ view thread
https://support.rockwellautomation.com/app/answers/answer_view/a_id/17911 Check whether the .LEN of the STRING variables in your program have a value > 82 or a negative value. ------------------------------ Ian Shaw Riverside Automation, Sheffield, UK If I've helped you, please Like ...
Posted By Ian Shaw Jul 14, 2025 03:27:00 AM
Found In Egroup: Automation Control
\ view thread
That sounds very puzzling. The rung-condition at the output of the COP instruction always matches the rung-condition at the input, so if the COP instruction runs than the FLL should too. Try adding some debug bits to prove what is happening. Try putting the COP and FLL on different branches ...
Posted By Ian Shaw Jun 09, 2025 05:54:00 AM
Found In Egroup: Automation Control
\ view thread
I don't know why it isn't reporting which task is the problem. You could try comparing the Last or Max scan time with the configured Watchdog time on each task's Configuration tab to see if any watchdogs have been exceeded. One would expect the Last Scan Time to exceed the Watchdog on the ...