List of Contributions

Timothy Koski

Contact Details

Timothy Koski


My Content

1 to 7 of 7 total
Posted By Timothy Koski Feb 25, 2022 07:37:00 AM
Found In Egroup: Networks and SecureOT
\ view thread
Thank you for your feedback. It was discovered that 2 pins s had been damaged/bent as shown in the attached pic. Pins were repaired and all is well!
Posted By Timothy Koski Feb 24, 2022 12:24:00 PM
Found In Egroup: Networks and SecureOT
\ view thread
I'm working with someone having a problem with a 1756-EN2T card that is giving the following message: Module reported general error status is: (16#1F) I haven't been able to find out anything on this error code. Bad card? Wrong card configured? I was only given a the following screenshot of the error ...
Posted By Timothy Koski Feb 24, 2022 12:23:39 PM
Found In Library: Networks
Posted By Timothy Koski Jan 25, 2022 10:38:00 AM
Found In Egroup: Networks and SecureOT
\ view thread
Daniel, Thank you for your reply. ​We seem to have cleared up the problem replacing the EN2T and patch cable, and updating the I/O trees to reflect a corrected communication path through an EN2T rather than a previous ENBT. We are also in the process of having direct cabling between the EN2T and the ...
Posted By Timothy Koski Jan 25, 2022 10:26:00 AM
Found In Egroup: Networks and SecureOT
\ view thread
Thank you for your reply. Both ends are set to 100MB Full duplex, but I will have ​it reverified. Thank you, Tim
Posted By Timothy Koski Jan 25, 2022 10:22:00 AM
Found In Egroup: Networks and SecureOT
\ view thread
Lesley, Thank you for your response. The cabling between the stratix and the EN2T card consists of a short patch cable from the EN2T to a port jack on the cabinet wall, Cat5e cable in conduit between the 2 cabinets to a port jack on the wall of the other cabinet, and then a short patch cable to the ...
Posted By Timothy Koski Jan 23, 2022 02:36:00 PM
Found In Egroup: Networks and SecureOT
\ view thread
We have 2 CLX processors communicating through a stratix switch passing data using produced/consumed tags. 1 processor is an L83E and the other is a L72 both running version 30.11 firmware. They are connected to the stratix switch through an EN2T v11.01 located in their racks. The EN2T on the L72 end ...