List of Contributions

Rominaldo Macaambac

Contact Details

Rominaldo Macaambac


My Content

1 to 20 of 40 total
Posted By Rominaldo Macaambac Mar 12, 2024 04:39:00 AM
Found In Egroup: Advanced Software
\ view thread
On my Asset Center I have error when taking backup for Asset Inventory but for others like Logix5000, FTView SE, Stratix Switch, and ME all works fine when taking Disaster Recovery. License also available (Base Server, Disaster Recovery, Asset Inventory).
Posted By Rominaldo Macaambac Mar 12, 2024 04:16:00 AM
Found In Egroup: Advanced Software
\ view thread
Yes Sir you're right I enabled the WSUS to download some updates to be able to install latest Symantec Antivirus software. Now after running the command you have given it works like a charm. Thanks a lot.
Posted By Rominaldo Macaambac Mar 07, 2024 06:22:00 AM
Found In Egroup: Advanced Software
\ view thread
Help please as I cannot open the graphics file (.gfx) from FTView Studio, before it's working fine and then suddenly cannot open anymore. Take note that HTTPS is not enabled so something in IIS have issue but in IIS Manager I can open ServerName\Sites\Default Web Site
Posted By Rominaldo Macaambac Feb 04, 2024 06:57:00 AM
Found In Egroup: Automation Control
\ view thread
Is there a new version of Logix Clock Update Tool that are using FT Linx instead of RS Linx Classic?
Posted By Rominaldo Macaambac Jan 31, 2024 02:44:00 AM
Found In Egroup: Advanced Software
\ view thread
Is there any option for Importing or Exporting Historian Points?
Posted By Rominaldo Macaambac Jan 26, 2024 03:49:00 PM
Found In Egroup: FactoryTalk Optix
\ view thread
Hello, I forgot to mention that the option "Disable switch to other application" is selected so SendKeys is not working. I saw also from Technote regarding VBA to send it to foreground and it works for Alarm Log Viewer but for the runtime client file it doesn't work.
Posted By Rominaldo Macaambac Jan 26, 2024 06:32:00 AM
Found In Egroup: FactoryTalk Optix
\ view thread
I have a Client Station where I want to run multiple client files (e.g. 5 different client files) and in my runtime window I have a button that if pressed it will switch to other running client, same like a functionality of Alt+Tab. Need help on how to achieve that functionality.
Posted By Rominaldo Macaambac Jan 22, 2024 01:12:00 PM
Found In Egroup: Advanced Software
\ view thread
Hello thanks a lot for the information. It means there's no option to have my SQL server redundant meaning 2 PC's with SQL Server-1 and SQL Server-2 installed and configured in redundant mode. ------------------------------ Rominaldo Macaambac ------------------------------
Posted By Rominaldo Macaambac Jan 22, 2024 01:28:00 AM
Found In Egroup: Advanced Software
\ view thread
Hello, I have only Server-1 & Server-2 where I install SQL on both servers but the database is only created on Server-1 (because FT Directory is on my Server-1) so when i shutdown the Server-1 I cannot access anymore the database and my Alarm History is not working anymore. By the way, server redundancy ...
Posted By Rominaldo Macaambac Jan 21, 2024 07:36:00 AM
Found In Egroup: Advanced Software
\ view thread
I need help as this is my first time to use Asset Center and I don't have any background about this or training. First, where should I install Asset Center in Operator Station or Engineering Station? Below list are my 3 licenses for Asset Center. FactoryTalk AssetCentre Base FactoryTalk AssetCentre ...
Posted By Rominaldo Macaambac Jan 21, 2024 07:28:00 AM
Found In Egroup: Advanced Software
\ view thread
I have FTView SE Network Distributed and I configured my databse (SQL) for alarm history logging and it works fine only for Server-1 but when I shutdown my Server-1 to take over my Server-2, my alarm history is not working anymore. Need help for other settings as I cannot find database redundancy option ...
Posted By Rominaldo Macaambac Jan 02, 2024 06:07:00 PM
Found In Egroup: Advanced Software
\ view thread
Hello, it is workgroup and it's communicating already by using same username & password. But I need to make it different like for Engineering Station & Servers it will have same password and for Operator Station it is different password also. So how it will be possible? P.S The existing FT View SE ...
Posted By Rominaldo Macaambac Dec 23, 2023 08:22:00 AM
Found In Egroup: Networks
\ view thread
I have 5700 Stratix switch, can I make REP protocol and connect to my I/O tree and make a ring topology? I knew DLR is available but other than that I need to used REP also as a separate ring. EDIT: moved to Networks community -FL ------------------------------ Rominaldo Macaambac -- ...
Posted By Rominaldo Macaambac Dec 21, 2023 06:37:00 AM
Found In Egroup: Automation Control
\ view thread
I have two Redundant L81E controller with its own Remote Ethernet I/O rack and a Common Rack both are configured in the two redundant CPU. Both of them are in Ring Topology and the Common Rack are interconnected thru a Switch (2pcs). When I connect the Common Rack to both of the CPU it gives me erro ...
Posted By Rominaldo Macaambac Dec 20, 2023 02:27:00 PM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Now it works perfectly without even 1s interruption. Another switchover test remaining for my redundant HMI, there's more or less 3s fluctuation when I shutdown the primary HMI server, but if I manually switchover either the HMI, Alarm, or Data Server it's bumpless. Are there any settings to fine tune ...
Posted By Rominaldo Macaambac Dec 18, 2023 03:23:00 PM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Thanks a lot I will try this configuration by tomorrow. :) ------------------------------ Rominaldo Macaambac ------------------------------
Posted By Rominaldo Macaambac Dec 18, 2023 01:45:00 PM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
Thanks for the info, my configuration is already the same as what you suggested but I'm using same IP address for ethernet cards. Our clients has commented that there should not be even 1s interruption during switchover because they said it should be same as the existing (v5.10). But the existing they ...
Posted By Rominaldo Macaambac Dec 18, 2023 09:41:00 AM
Found In Egroup: Drives, Motion Control & Low Voltage Products
\ view thread
I have FTView SE v13 Distributed and Redundant L81 CPU, when I switchover the CPU the communication lost for about 20s then resume, is this normal or any other settings to configure to rectify this issue? ------------------------------ Rominaldo Macaambac ------------------------------
Posted By Rominaldo Macaambac Dec 17, 2023 05:41:00 AM
Found In Egroup: Advanced Software
\ view thread
Help please on this function alm_tags_inalm() and alm_tags_unack() from FTView SE v5.10 to v13 what is the corresponding function? ------------------------------ Rominaldo Macaambac ------------------------------
Posted By Rominaldo Macaambac Dec 13, 2023 10:10:00 PM
Found In Egroup: Installation & Activation
\ view thread
In the FTAM of Client PC I already pointing the PC which is hosting the activations but I cannot see the activations in the Client PC unless I will enable the Codemeter Network Server in the PC hosting the activations which is my HMI Primary Server. And because of this I have another question, how ...