List of Contributions

Sol

Contact Details

Sol


My Content

1 to 20 of 37 total
Posted By Sol Nov 26, 2024 09:51:00 PM
Found In Egroup: Automation Control
\ view thread
Hi, I have an application which charts a pressure value with the chart object, working well, and have a print_display button for the user to generate a pdf of that screen. Is it possible for me to automate that print from the plc so that if they forget to do so, then the logic routine can do it for them, ...
Posted By Sol Sep 26, 2024 11:43:00 PM
Found In Egroup: Automation Control
\ view thread
I'm sorry it took so long to see your reply fuzzy logic, my mistake. I've used many 820 controllers but failed to realise that the 830 (which one would have assumed was as good if not better than the 820) also had ethernet and a micro sd slot - it seems I was wrong and it was actually crippled with only ...
Posted By Sol Sep 22, 2024 04:41:00 AM
Found In Egroup: Automation Control
\ view thread
Hi Gianlu and thanks for replying. I have read that article before and still have a question, it is that the control iterates through all data series whether they are used or not, which takes a considerable time (if the maximum 500 points are used in the dataseries UDT) so the display takes a long time ...
Posted By Sol Sep 06, 2024 12:06:00 AM
Found In Egroup: Automation Control
\ view thread
Hi folks, after using the Chart control ActiveX and finding the long delays when switching hmi displays while this control is displayed, I watched a video on the newer ChartEX control where the connection is per-pen rather than per chart. I'm using ftview me 12.0 and wonder if anyone can tell me the ...
Posted By Sol Aug 13, 2024 12:26:00 AM
Found In Egroup: Automation Control
\ view thread
It was not accepting THIS and I had to manually fix the _EWEB_path tag to $01xxxxx etc after checking what it had been automatically set to in the first example. This re-established the normal behaviour, as in the first PLC. No idea how it became changed on importing the routine, but now back to where ...
Posted By Sol Aug 01, 2024 07:34:00 AM
Found In Egroup: Automation Control
\ view thread
Hi all, I'm using the RA example code to send data to an Ethernet connected printer, using unconnected MSG over TCP/IP. On the first PLC - a 1756-L83E I built my own code around the example rungs which themselves set up create_sock_MSG, connect_MSG, write_data_MSG and delete_socket_MSG etc ...
Posted By Sol May 01, 2024 08:39:00 AM
Found In Egroup: Automation Control
\ view thread
Thanks both of you, I realise now I was over thinking it - just push the decimal value to the SINT array pointer where you want it to be, and it gets sent as an ASCII byte value regardless of whether it was a decimal or not, doh. You don't know, until you know, right! I really appreciate the clear ...
Posted By Sol Apr 30, 2024 07:09:00 AM
Found In Egroup: Automation Control
\ view thread
Hi all, I create an array of hex byte char values in a string which of course fills the SINT array, such as $EB$00$04$00 and then convert another value in decimal to a hex string, lets say 7F, then I need to move that value to the next location in the SINT array so the whole string reads $EB$00$04$00$7F ...
Posted By Sol Jan 11, 2023 05:40:00 AM
Found In Egroup: Advanced Software
\ view thread
Hi, I have FT Metrics comprising of RSBizware v11.50 and ReportExpert 3.2.00 along with SQL 2012 64 bit SP4. I want to update Metrics to V13.00 but it is asking me to uninstall V11.50 first (ReportExpert and RSBizware are of course installed separately but for clarity I refer to them as FT Metrics) ...
Posted By Sol Jun 07, 2022 09:15:00 AM
Found In Egroup: Automation Control
\ view thread
The easiest way is to fit a ProSoft MODBUS card to your CLX backplane and use that to handle the comms. ProSoft configuration tool is free, and lets you define the client device IP address and the registers you want to read from, or write to. It can handle 600 read registers and 1000 write registers. ...
Posted By Sol Jun 07, 2022 09:09:00 AM
Found In Egroup: Automation Control
\ view thread
Have you tried using Ethernet to connect, and having RSLinx running then using BOOTP to find and configure the IP address of the 830 first? It can also be configured from an SD card with a file on it called ConfigMeFirst.txt (details are online) I always found USB to be unreliable for various reasons ...
Posted By Sol May 09, 2022 08:31:00 AM
Found In Egroup: Automation Control
\ view thread
The global supply shortage of silicon due to Covid, Chinese lockdowns, ramped up EV manufacturing, it all has an impact on what even Rockwell can get their hands on. One manufacturing company I know, needed a small I2C chip and a PIC Micro-C of some sort, they found out that Bosch washing machines already ...
Posted By Sol May 09, 2022 04:45:00 AM
Found In Egroup: Automation Control
\ view thread
We are a large product manufacturer who use Rockwell parts in our own machinery, I am on a 31 week lead time for a Control Logix PLC and analogue I/O in the UK, direct from Rockwell via Routeco. But also hear from German colleagues that Siemens is not much better. ------------------------------ Zion ...
Posted By Sol Mar 25, 2022 10:31:00 AM
Found In Egroup: Automation Control
\ view thread
I will do, the printer is offline but when I get the machine back on I'll try all of the above. The one in post #24 was PLC to EWEB.​ ------------------------------ Zion ------------------------------
Posted By Sol Mar 25, 2022 05:31:00 AM
Found In Egroup: Automation Control
\ view thread
Here is a packet sent by PuTTy in RAW mode, to which the printer would respond (example sent to eweb in the mode used by the printer with no CR but just to see how the PuTTy packet differs) ------------------------------ Zion ------------------------------
Posted By Sol Mar 25, 2022 05:29:00 AM
Found In Egroup: Automation Control
\ view thread
Here is the packet sent from the PLC, captured in Wireshark, you can see I sent the CR as $r ------------------------------ Zion ------------------------------
Posted By Sol Mar 24, 2022 12:01:00 PM
Found In Egroup: Automation Control
\ view thread
Thanks Derek. So that's where I'm at, using prebuilt code from RA that works perfectly to a TCP server app (eweb from RA is such a tool) and both PuTTy and the PLC can send messages to it, working perfectly. Using UDP, or TCP, all good. The weird thing is, the Videojet printer responds to PuTTy in ...
Posted By Sol Mar 24, 2022 11:05:00 AM
Found In Egroup: Automation Control
\ view thread
Hi Derek, thank you for taking the time to respond with such a comprehensive reply. I'll have a look into the method and see what I can do with it. This does seem as robust as possible when dealing with older ascii devices. The code I've put together now works to the Rockwell eweb app, in TCP or ...
Posted By Sol Mar 19, 2022 03:14:00 AM
Found In Egroup: Automation Control
\ view thread
Yes, I had slipped when inputting the IP address so it stopped working all together but when I found that typo, it started working again but not reliably. Often I would get extended error 0044 which is not in the sockets documentation. Searching that error on the portal led me to a technote on specifying ...
Posted By Sol Mar 18, 2022 10:10:00 AM
Found In Egroup: Automation Control
\ view thread
Quick update for anyone else following this topic, Question Why am I getting the following error codes 16#00f or 16#0000_0044 when making a Socket Message using CompactLogix or ControlLogix Controller? 5580 Controllers the path should be of the format $1F$00$00$00 for the local ...